Part Number: TDA2E Tool/software: Hi TI Expert,
We want to konw what is L4_CFG_IA_IP0 Region of TDA2E used for, can i change the register value of L4_CFG_IA_IP0?
And what will happen if some register value of L4_CFG_IA_IP0 is changed by user ?
…
Part Number: TDA2P-ACD Other Parts Discussed in Thread: TDA2E Tool/software: Hi Everyone,
Do we have a TDA2E to TDA2P (or H) migration guide? my customer needs to understand the SW and HW differences for each.
Part Number: TDA2E Tool/software: Case A:
// config GPIO_1 to output mode
GPIODirModeSet(gpio_1, GPIO_DIR_OUTPUT);
// set GPIO_1 to HIGH
GPIOPinWrite(gpio_1, GPIO_PIN_HIGH)
// The high level duration here is 350ms by The oscilloscope.
// It…
Part Number: TDA2E Tool/software: Dear Team,
For one of our project we are debug an PLL lock issue in Serializer and Deserializer. To debug the issue we need to monitor DE(Data Enable) pin from Serialiazer, to control particular pin need to drive…
Part Number: TDA2E Tool/software: Hi :TI
After quantization, the object detection model experiences a loss of accuracy during on-board inference, with a decrease of approximately 4.5% compared to the PC-side performance. Could you please advise on how…
Part Number: TDA2E
Tool/software:
Hi,
TDA2ex VSDK3.05
DRAM: 1 GiB
uboot laod load dra7-ipu2-fw.lzop, dtb, zImage, mount rootfs.
I did it according to the following method. 1.uboot load dra7-ipu2-fw.lzop Other nuclei are not needed, I have…
Part Number: TDA2E Tool/software: Dears,
Our project uses TDA2x and TC397 Ethernet direct connection, with TDA2x internal switch as shown in the screenshot.
My question is whether the connection between TDA itself and the external environment should…
Part Number: TDA2E HI TI:
THE SMPS3 of TPS65917 is use for VDD_GPU of TDA2E,
and i need increase the voltage of VDD_GPU about 50mv,
How do I achieve this?
Part Number: TDA2E Tool/software: HI:TI
What command does tidl_tb.c under the /ti_components/algorithms/REL.TIDL.01.01.03.00/modules/ti_dl/test/src path compile to generate an executable file? I am /ti_components/algorithm/REL TIDL. 01.01.03.00 / modules…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Tool/software: Dears,
Our project uses TDA2x and TC397 Ethernet direct connection, with TDA2x internal switch as shown in the screenshot.
My question is whether the connection between TDA itself…