Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Hi, Support
The processor we use is TDA2 ECO 23*23. My video output resolution is 1780*720, When I RGB output video, everything is normal. When I yuv output, a part of the picture is green in external…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 hi, ti support
The processor we use is TDA2 ECO 23*23. There are 4 cameras in our system. The interface connected to the deserializer (DS90UB960) is the mipicsi interface.
The resolution…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 This is my import log in TIDL,
4744.quantize_log.txt
PS E:\hhq\quantize\importTool> .\tidl_model_import.out.exe .\tidl_import_caffemodel.txt
=============================== TIDL import…
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 Hi,
I have some questions I want to ask,
I want to change the input format of TDA2. Where do I need to change it? For example, I want to change YUV422SP to RGB888
Part Number: TDA2E Other Parts Discussed in Thread: DRA726 Hello!
I have a J6ECO/TDA2E EVM CPU BOARD with a DRA726 processor. A few questions:
1. Can I use J6ECO/TDA2E with PROCESSOR_SDK_VISION? or I need another SDK. 2. If I will use PROCESSOR_SDK_VISION…
Part Number: TDA2EG-17 Linux suspend to disk with hibernate on TDA2EG-17
We are developing 360 SVM product with VisionSDK on TDA2EG-17, but it need 8s to output 2D stitched image view from cold start.
Our customers want our 360 SVM products to output…
Part Number: TDA2E Tool/software: TI C/C++ Compiler Hi,
Can the watchdog of the TDA2ex chip record the type of the last system restart? Such as: watchdog timeout restart, reboot restart and power failure restart, etc.
Thanks!
Part Number: TDA2E Hi Expert,
Could you help confirm whether if TDA2Ex could support 2 cameras via the MIPI interface?
and provide me the Quotation of TDA2Ex (SOC) ? Thanks.
Thanks
Daniel
Part Number: TDA2E Other Parts Discussed in Thread: TDA2 There is such a problem in the customer's project requirements.
Multiple VLANs need to be configured on TDA2EX SOC , but they all use the same IP address. What kind of configuration do you have…
Hi Yumei,
You can refer to FAQ 21 and 22 in the user guide for the same.
As I said earlier, run DectectionOutputLayer on DSP and rest of the all the layers on EVE in the SSD network to get optimal performance, if you have already tried this combination…