Part Number: TDA2P-ACD Other Parts Discussed in Thread: TDA2 Hello,
My customer wants to move their platform form TDA3 to TDA2 due to get more computing power.
but it is very hard to get the EVM. How they can get the EVM?
www.ti.com/.../TDA2PXEVM…
Part Number: TDA2P-ACD Hi TI Team,
We are evaluating a camera configuration that provides 16-bit uncompressed RAW Bayer data to the TDA2P.
From the TDA2P TRM, we understand that:
CAL supports RAW16 pixel packing/capture. IPIPEIF supports up to 16…
Part Number: TDA2P-ACD Hello TI team
I am currently working on enabling I2C5 on the TDA2PHVRQACDQ1 platform. However, I am encountering issues with interrupt handling and core stability.
I have configured the following registers for clock gating and…
Partha,
Unfortunately, only the SDK examples are supported. Do you mean that you are writing your own Mailbox drivers? -or- Are you using the drivers from this SDK?
Partha Hazarika said: TI SDK 03_05
This is the RTOS SDK version number right?
…
Part Number: TDA2P-ACD Hello,
In my design VIN2A_D(0-23) connected to Serialiser. Whether those signals with pins are configured as Output, Input or IO?
Thanks,
Manikandan M
Part Number: TDA2P-ACD As per the datasheet, there is no information regarding the output skew data for TX group signals, is there anything else that I need to refer from datasheet to get the output skew(jitter) deatils? Meanwhile can you please let me…
Part Number: TDA2P-ACD Other Parts Discussed in Thread: TDA2E Tool/software: Hi Everyone,
Do we have a TDA2E to TDA2P (or H) migration guide? my customer needs to understand the SW and HW differences for each.
Part Number: TDA2P-ACD In the data sheet of TDA2Px, tc(DDR_CLK) is mentioned as 2.5ns max in table Table 7-42,which translates to a frequency of 400MHz, which means that we can run DDR3 data at maximum 800Mbps, but it supports DDR3-1333 and DDR3-1600…
Part Number: TDA2P-ACD Hello,
In the datasheet, Table-110 mentioned 1.05 ns for output setup & hold time for RGMII0 (1000 Mbps). If i consider this value means, 2.1 ns is for output setup & hold time. In my PHY configuration have 1 ns for setup time…