Part Number: TDA3MV I'm outputting camera data coming into the ISS port on the TDA3 to DSS via the DSP.
I want to upscale the data output to the DSP. Which one should I use?
dss_m2mwb? or iss_m2mresizer?
I need some advice.
Part Number: TDA3MV Hi TI Team,
I am currently working with the TDA3MARBABFQ1 SoC and would like to request some technical information and resources related to this device.
SDK Availability
Please provide the Software Development Kit (SDK…
Part Number: TDA3MV Tool/software:
Hello.
I encountered an issue while writing firmware to flash on the TDA3 using JTAG and the flash writer. According to the CCS log, there seems to be no problem with the JTAG connection and initialization. However…
Part Number: TDA3MV Tool/software: Hello
I use ISS CPI Capture.
I want to get the data between the lines.
When hsync is high, the active image (one line) appears, then hsync drops to low and about 25 pixels more appear, which contains the data I…
Part Number: TDA3MV Tool/software: Hi Team,
My customer has some issue while they are using TDA3MVRBFABFRQ1
with 2pcs DDR3(K4B4G1646E-BNCB)
Here's the log they get.
What can be the cause of this problem?
if you need more data to analyze this…
Part Number: TDA3MV Tool/software: Hello
I want to set iss cpi_pclk polarity. It says in TRM that it can be set, but I couldn't find the register information.
It's hard to find the corresponding code in the sdk either.
Thank you
Part Number: TDA3MV Tool/software: Here is the translation of your question:
Hello, I am working with PROCESSOR_SDK_VISION_03_05_00_00. I am currently using UART2. I would like to use UART1 as well, and I am wondering where to enable UART1. From what…
Part Number: TDA3MV Tool/software: Hi,
How can we evaluate the power consumption of TDA3x? How do we find the power estimation software, TDA3xx Power Estimation Spreadsheet?
Best Regards
Tom