Part Number: TDA4AEN-Q1 Hello Ti Experts,
1 When calling the Fls module to erase the interface, it will be blocked in the SchM_Exit_FLs_EXCELCLUSIVE_AREA function, and the code for this function is not displayed. I would like to ask what is the reason…
Part Number: TDA4AEN-Q1
Hello Expert.
As titile description.
Does TDA4AEN support CAN BUS TEC (Transmit Error Counter) / REC(Receive Error Counter) ?
If the answer is "yes", where is sample code or demo?
If the answer is "no", Does it mean this…
Hi Tsai,
YT Tsai said: (1) We only need point cloud and object tracking data processing, but don't need the graphic service or GPU. We use TDA4"A"EN. That means OpenVX is also unnecessary for us. Is it possible to develop without OpenVX?
Well, OpenVX…
Part Number: TDA4AEN-Q1 Other Parts Discussed in Thread: SYSCONFIG , TDA4VM Hello Team,
I am working on a TDA4AEN (J722S) board using the C7x DSP with the Processor SDK RTOS.
I would like to clarify whether the C7x on TDA4AEN/J722S has direct access…
Part Number: TDA4AEN-Q1 Other Parts Discussed in Thread: SYSCONFIG , , UNIFLASH
The J722S TRM incorrectly states that GPIO1_52 through GPIO1_71 do not support interrupt functionality.
In reality, these pins do have interrupt capability but require…
Part Number: TDA4AEN-Q1 1 Debugging found a bug in the Fls_Brd_NOR. c interface of the MCAL driver Fls_Brd_NOR. c where the next write was performed without checking if the flash was complete, resulting in occasional data write failures. Solution: After…
Hi Quan,
Is this iros_app_capture your custom application ? could you provide any sample code that could reproduce the issue from our end.
quan.li said: Is this issue known for J722S + current PSDK/TIOVX stack with vxSwapImageHandle and UYVY single…
Part Number: TDA4AEN-Q1 Dear TI Support Team,
I am working with the TDA4AEN J722S controller. Initially, I successfully flashed the SDK “Hello World” examples on the MCU R5F core and verified that the software executed correctly with the expected output…
Part Number: TDA4AEN-Q1 Other Parts Discussed in Thread: FFTLIB Dear Expert.
These question direct comes from customer.
I think this is extenseion discussion from this thread.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum…
Part Number: TDA4AEN-Q1 Hi, I'm jin-mook in Yura corp.
Is there a function in vision_apps to encode the current video and then transmit it via Ethernet?
Or is there a way to check the video output via Ethernet?
If possible, please provide some examples…