Part Number: TDA4VEN-Q1 We are performing power-up timing validation for the TDA4VEN-Q1 system-on-chip. Per the official TDA4VEN-Q1 user manual requirement, waveform H (corresponding to VDD_CORE supply) should begin oscillating/activating prior to waveform…
Part Number: TDA4VEN-Q1 Hello,
Regarding the TDA4VEN I have the following questions:
USB3SS (USB1) Subsystem: For the TDA4VEN-Q1 USB3SS (USB1) subsystem, does Device/Peripheral mode support SuperSpeed (5 Gbps), or is Device mode limited to High…
Hi Aditya,
Aditya Sankhe said: Can you confirm the power-domain / rail assignment for these four balls (B7, E8, D10, E13) — specifically that MCU_ERRORn and MCU_PORz are on VDDS_OSC0 (1.8 V only) while MCU_RESETz and MCU_RESETSTATz are on VDDSHV_MCU…
Hi Gang,
Gang Hua said: I am not sure what you mean exactly here.
As the lighting was quite bright at the time, the noise in the photograph is not particularly noticeable. Therefore, a side-by-side comparison of the images taken before and after applying…
aurora gao said: EE started up correctly using your method. The problem was with the SDK's compilation environment.
Thanks for the confirmation!
Glad to hear that it is working well now on your side.
Part Number: TDA4VEN-Q1 We would like to know how to connect and configure dual monitors on the TDA4VEN board. Could you please share the relevant documentation, user guides, or example implementations for setting up a dual-display configuration?
Part Number: TDA4VEN-Q1 Does the differential level swing of TDA4VEN/J722S video output interface OLDI support adjustable driving strength, with a default swing of 350mV? I would like to inquire if it is possible to adjust it to 250mV or reduce the driving…
aurora gao said: In fact, I observed that this effect is caused by the exposure time and gain, and is somewhat similar to the results obtained by increasing the auto exposure target value. At this point, the exposure time is already at its maximum, and…
Part Number: TDA4VEN-Q1 Problem Description:
We are developing GPIO interrupt functionality on the MCU domain of the TDA4VEN using SDK 11.0.0 with TI's provided FreeRTOS. We have two hardware revisions and are encountering interrupt loss on both:
…
Hi Toshiki,
toshiki kouzai said: The reason why STREAM1 and STREAM2 were enabled is due to the new driver settings, and the problem was that all channels on the DES#1 input port were enabled.
Sorry, but when you say STREAM1 and STREAM2, do you mean…