Hi Ying,
Ying.li said: What do the horizontal and vertical coordinates of these three graphs represent?
That is Cb and Cr as in the plot.
Ying.li said: Why is it divided into four grayscale levels? I
I suppose by four grayscale levels you mean you 4 lines…
Part Number: TDA4VM Tool/software: Hi,
While I was performing a secure boot, the following error occurred.
Subsequently, every time I reached this point, a restart was initiated.
I would like to ask: 1. Is the continuous restarting related to the memory…
Part Number: SK-TDA4VM Tool/software: Hi SK-TDA4VM Champ !
Can you please check if any other reason is available of revision history from A to A1?
Thanks.,
Best Regards,
Jack
Part Number: TDA4VM Tool/software: Hi,
We want to develop a secure boot function in the SDK 10.0 version. Currently, we are using SD card boot. When using the keywriter tool, MCU1-0 reported the following LOG:
From the code perspective, the source…
Hi dhivakar sriram.M ,
I am glad to hear that your issue has been resolved. Please mark my initial response as having resolved your question and I will close this thread.
Thank you,
Fabiana
Part Number: SK-TDA4VM Tool/software: We are performing UDP performance testing on the QNX system, using a ping-pong mode for the test. For the ping side: It only sends UDP packets and waits for responses from the pong side. After receiving the response…
Hi,
Hasan Aarzoo said:
Priority of Port using PORT_PRI (13-15 bits)
Vlan ID of port using PORT_VID (0-11 bits)
then how it port priority is set by making MAC Port and HOST Port member of ALE Unknown VLAN (ALE is in VLAN Aware mode)?
CPSW should be in VLAN…
Part Number: TDA4VM Tool/software: backgroud: SBL: PDK8.4 MCU1_0: PDK10.1 issue: The MCU can not boot that loop in brsStartupZeroInitLoop() in .asm file, as the follow photo:
We found that the MCU1_0 enter point address is not right with the SBL. Any idea…