Part Number: TDP0604 HI TEAM
I want to ask if there is a problem with my current design?
Please see the attachment
UBIQCONN_HDMI Level Shift Hybrid redrive_ted0604i_20230314_01.pdf
Part Number: TDP0604 Hi,
I am using TDP0604 as an HDMI retimer in a video monitor and have two questions.
Question 1. There may be a case that HDMI signal is applied to the device while the DC power of the device is off. I am concerned that the current…
Part Number: TDP0604 Hi,
I had design TDP0604 for HDMI2.0 output.
I set control method to I2C control mode.
But I did not find these parameter default value. Please help to provide this information, thanks.
1) Lane swap. Normal or reverse
2) Receiver…
Part Number: TDP0604 Hello,
I have a TDP0604 in a DP tp DP linear redriver configuration set over I2C. I am trying to tune the EQ settings for my losses on board via I2C registers. The register sets have explicit 0-15 bit for EQ settings on lanes D0-D2…
Thanks, Zach. But I don't think you've fully answered my questions.
Roy Hsu said: What's the step of each setting in SLEW_3G and SLEW_6G? (How many V/us?)
Why are the four highlighted fields not 3'b000 ~ 3'111 since I believe there are total…
Hi Zach,
Yes, my question is why we have HPDOUT_SEL pin in general.
David (ASIC) Liu said: In pin-strap mode, the HPD_OUT is always push/pull.
Since HPD_OUT is always push-pull in pin-strap mode and selecting between open-drain and push-pull in I2C mode…
Part Number: TDP0604 Hi,
We use the TDP0604 on a custom board and implement it as an HDMI RX. The image receiving destination is FPGA. As a result of verification with a custom board, depending on the device to be connected, the bias voltage may be output…
Dear David.
May I ask you one last question?
Looking at the TDP0604 datasheet and reference circuit, a circuit is shown that allows
an external DDC buffer to be used.
Does this mean that the TDP0604 DDC buffer is often not available, as in this case…