Part Number: TUSB1064 Other Parts Discussed in Thread: TUSB8044 , TDP0604 , , TUSB8044A , SN65DP159 Hello,
I am working on the HUB design with 2x USB 3.X and 1x HDMI outputs.
I selected the TUSB8044 for HUB (even there are 4x USB3x).
Also, I need to find…
Oh I see, sorry for the miscommunication. What HDMI version are you using? Here are some possible redrivers and retimers you can use.
Retimer:
TMDS181: https://www.ti.com/product/TMDS181
Redriver:
TDP0604: https://www.ti.com/product/TDP0604
TDP1204: https…
Wes
For USB2.0, you can use TUSB211A, https://www.ti.com/product/TUSB211A .
For USB3.0, you can use TUSB501, https://www.ti.com/product/TUSB501 .
For HDMI2.0, you can use
TDP0604, https://www.ti.com/product/TDP0604 for AC/DC coupled input
TDP158, https://www…
Ravi
For HDMI2.0, you could use TDP0604, https://www.ti.com/product/TDP0604 as it supports both source and sink application.
For both TDP0604 and TMDS1204, both are re-driver not re-timer. Both will accept PRBS7 data pattern as long as the input condition…
Hi Arabella,
DS125MB203 is intended to be used for 10G ethernet, PCIe3.0, and SAS2/SATA3 applications. It is not designed to be used for HDMI applications.
I recommend you use TDP0604 or TMDS181 in combination with HD3SS215 or TS3DV642 instead. These devices…
Hi,
They can use TDP0604, which is our latest HDMI re-driver. The EVM is available at this link, https://www.ti.com/product/TDP0604#design-development .
Thanks
David
Part Number: TMDS1204 Other Parts Discussed in Thread: TDP1204 , TDP0604 Hello Experts, My customer would like to know whether a timing relationship between VCC and VIO when device is turned on. Does this device has any restriction for turned on timing between…
Hi, Silvia
If you need a HDMI re-driver that can support 1.8V I2C, please take a look at the TDP0604, https://www.ti.com/lit/ds/symlink/tdp0604.pdf . It has a separate VCC 3.3V and VIO supply. When VIO is between 1.5V and 2.5V, then the TDP0604 I2C will…
David
DP141 will not work as a HDMI2.0 re-driver. For HDMI2.0 re-driver, please take a look at the TDP0604, https://www.ti.com/product/TDP0604 .
Thanks
David