Part Number: THVD1400 Other Parts Discussed in Thread: THVD1420 , Hello
I have a question about the THVD1400 and the THVD1420: in the datasheet there is a pull up to Vcc for the R pin.
We want to add a LED on this pin and use also the pull up as…
Part Number: THVD1400 Other Parts Discussed in Thread: ISO7741 , Tool/software: Hi team,
Could you pls provide UL\TUV \ CCC or CQC Certification of THVD1400DR ? thansk
Part Number: THVD1400 Hello, I am interested in using the THVD1400 in a system with multiple modules The application is a bit specific and requires a very low bus input current when the transceiver is not used.
The datasheet specifies the maximum bus…
Part Number: THVD1400 Hi,
I am looking to use the THVD1400 RS485 Transceiver in a design where the RS485 bus will be connected to third party equipment and I will not have any infomation about any biasing arrangements of this.
I therefore plan to…
Part Number: THVD1400
Hi team,
I believe these capacitors are used as decoupling capacitors for power supply stabilization.
Are the capacitors marked with the red circles also required, or are the capacitors marked with the blue circles sufficient…
Part Number: THVD1400
I have a question about the THVD1400 and I hope you can confirm me my thoughts.
We want to supply the THVD1400 with +5V so that we will use this circuit as in the datasheet
We have a +3.3V microcontroller and I am wondering…
Part Number: THVD1400
Tool/software:
Hello E2E Community,
We are trying to improve the Surge & Transient immunity of our sensor nodes that are interfaced using THVD1400.
We have a TVS diode with following specifications - based on your expert…
Part Number: THVD1400 Dears:
Customer need TI help provide THVD1400DR latch off test current based on JESD78 .
You can refer to below reliability test report. It just shows THVD1400DR pass latch off test , but it doesn't provide test current .
THVD1400DR…
Part Number: THVD1400 Other Parts Discussed in Thread: SN65HVD75 Tool/software: HI,
The customer uses THVD1400 as the RS485 transceiver. Feedback power consumption is high and cannot meet the demand. Is there a recommended product with better power…
Part Number: THVD1400 Tool/software: Please suggest an SPI to UART converter which can act as master for IIM-42653 Gyroscope sensor , which communicates using SPI Protocol and functions as SPI Slave . looking for an IC which can : i) Functions as an SPI…