Hi Kiyoshi,
I believe I reviewed this schematic / block diagram on your other thread - here is a link to the thread as I go through the comments there.
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1128444/thvd1406-about-connection…
Part Number: THVD1426 Other Parts Discussed in Thread: THVD1406
Hi Team,
Customer would like to design THBD1426.
are external resistors required on VA and VB for auto-direction mode?
can customer not place 120ohm resistor between A and B?
thanks for…
Vidhya,
In the THVD1406, if D is left open/high for longer than tdevice-auto-dir, the receiver will automatically be enabled. So, on the THVD1406, you can tie both SHDN and RE high and control the driver and receiver using the D pin connected to the MCU…
Part Number: SN65HVD12 Other Parts Discussed in Thread: THVD1406 All,
Is it possible to hardwire the SN65HVD12 for Rx and Tx to always be active (DE = 1, RE_N = 0)? The FPGA does not have a spare pin to control remotely. Thanks!
Justin
Other Parts Discussed in Thread: THVD1426 , THVD1406 Dears
Does TI have an RS485 chip that automatically controls the input and output directions?
Replacement MAX13488
Thanks
Elsa Duan