Part Number: THVD1410 Tool/software: Dear Specialists,
My customer is considering RS485 transceiver and has questions.
I would be grateful if you could advise.
ーーー
(1) The THVD1410 has the Extended Common Mode notation, and the datasheet states that…
Part Number: THVD1410 Tool/software: Hi team,
As I know RS-485 can support 32 devices up.
So Ro of one device defined 12KR and 12K/32 then got 375R. if VCC=5V
5V/375R=13mA
PD=5V*0.013A=65mW Is correct?
HI Parker,
Thank you very much for your reply and I'm sorry to be late my response.
I told your reply to the customer and they understood it. The reply is very helpful for the customer and me.
Thank you very much again and best regards, Kazuya.
Part Number: THVD1410 Other Parts Discussed in Thread: THVD1452 , THVD1424 Hi
we are using the THVD1410 device in making a audio conference system
running the device at 3.3VDC.
Termination at the o/p (across A B pins) is of 120 ohm
Conference system is…
Part Number: THVD1410 What is the driver output current when unpowered, IO(off), and the driver output current when disabled?
I could only find the receiver output current when disabled in the data sheet.
Part Number: THVD1410 Hello,
I have this part THVD1410DR.
But X ray result is different from my previous order.
Could you please check and advise if this is a normal situation?
Thank you!
Part Number: THVD1410
Hello! I am a bit confused about the termination resistor requirement for THVD1410. The standard for RS485 is 120Ohm. In the datasheet though, the recommended value is 54Ohm. With a 120 Ohm termination resistor I am seeing 4V at the…
Part Number: THVD1410 Hi Team,
I am using THVD1410DR RS485 transceiver in my target board, the schematics of the RS485 is attached for your reference.
To test RS485 communication, I had connected target board with THVD1410DR transceiver to my PC with RS485…
Part Number: THVD1410 Hi team,
My customer use thvd1410, their signal rate is 500kbps, it's just the max for thvd1410, can it work? the number of devices is 32.
Thanks,
Colin
Part Number: THVD1410 Other Parts Discussed in Thread: THVD1450 , Hi team,
I have a stupid question...THVD1410‘s price is the same to THVD1450. As the THVD1450 have higher speed grade, why we choose THVD1410. That is, in which circumstance should…