Part Number: THVD1420 We are using MFR part no. SP3485EN-L/TR in our one of the product in Mbus-RS485 interface but we are facing some short circuit current flow in pin B to GND line. So can you conform weather this part no. have internal clamping or…
Part Number: THVD1420 Other Parts Discussed in Thread: MAX3223 , THVD4421 My system can be configured for RS232 or RS485. I'm wondering if it is possible to split a USART pin pair between THVD1420 and the MAX3223? I'm worried about leakage current and…
Part Number: THVD1420 Good morning,
I need the supply current of this part to interpret the max power consumption of this device.
Thank you,
Elizabeth Mikulas
Part Number: THVD1420 Hi expert,
Could you pls help share the THVD1420DRLR CAD symbols and 3D models for me? since the ti.com cannot down it,
BR,
Hangjie
Part Number: THVD1420 Hi Team,
Follow up on the E2E thread below. Our customer would like to know the supply current of the THVD1420DRLR if the device is connected to a load/network.
https://e2e.ti.com/support/interface-group/interface/f/interface…
Part Number: THVD1420 Other Parts Discussed in Thread: THVD1400 , Dear TEXAS INSTRUMENTS Team, I hope this message finds you well. I Want THVD1420DR this Product IBIS Model. Could you please Share Them. Thank you for your time and support. I look forward…
Part Number: THVD1420 Hi All,
I have a question about the THVD1420. I was unable to communicate via RS485 properly using the circuit diagram in the datasheet below.
When I changed the pull-up on the R pin to a pull-down, communication was successful…
Part Number: THVD1420 Hello,
The THVD1420DRLR chip has a pin virtual soldering problem, as shown in the following figure. Solder accumulates at the end of the chip pins, and there is a problem with the cross-section at the end of the pins that cannot…
Part Number: THVD1420 Hello, I want to confrim if THVD1420's internal failsafe still work with AC termination. THVD1420's failsafe function is just having negative Vth. When the bus is open with AC terimnation, I think both A/B inputs are just floating…
Part Number: THVD1420 Tool/software: Hey team,
Is Ios spec implying the need for the 10Ohm series resistors on A/B or something else? Are there internal protection that limits the current?
Thanks,
Cam