Part Number: THVD1424 Tool/software: Hello
I need an RS-422 IC that I can switch between full duplex and half duplex I found the "THVD1424" IC but officially, there is no source that this IC can work with the RS-422 protocol. Can I use this IC for RS…
Part Number: THVD1424 Other Parts Discussed in Thread: THVD1400 Hi, is there an ibis model for THVD1424? If not, is there a good placeholder part that can be used in the meantime?
Thanks,
Brendan
Part Number: THVD1424 Hi expert,
Could you please help confirm whether there is a device with the THVD1424 P2P Q1 version or other recommended PN of Q1 version? thanks.
BR,
Hangjie
Part Number: THVD1424 Other Parts Discussed in Thread: AM26LV32 , AM26LV31 Hello,
I am trying to understand the difference between RS485 and RS422. I have read as many TI app notes as I could find along with a few from other sources. I have a strong understanding…
Part Number: THVD1424 When using the THVD1424 in Half-Duplex mode, are collisions on the Z/Y TX/RX pins controlled automatically internal to the IC, when I can just keep both the TX and RX enabled all the time? Or do I need to use SW control (on /RE and…
Part Number: THVD1424 Hi team,
What is the maximum power rating of this device? Customers are concerned about the small size and integrated termination resistors.
Regards,
Goto
Part Number: THVD1424 Hi team,
The datasheet states the maximum data rate as below.
So, when SLR=Low, maximum 20Mbps is achievable. When SLR=High, then the date rate will be limited at 500kbps max even if the actual communication speed is 1Mbps. Is…
Part Number: THVD1424 Other Parts Discussed in Thread: AM26C31 , AM26C32 Hi,
I heard RS-485 is half duplex and RS-422 is full duplex, from electrical, they are same. So two RS-485 PHY can become a RS-422 inteface, and A RS-422 PHY can become a RS485 inteface…
Part Number: THVD1424 Hello team,
I received questions from the customer.
Under the following conditions, only the highlighted area has a high resistance value, is this a problem? Communication is working even if the resistance is high.
Half / Full…
Part Number: THVD1424 Hello For my design to use THVD1424 for half duplex (with H/F pin tie to High) application, shall the MCU I/O connect just to THVD1424 pin Y and Z (there is already internal connection within the IC to both transmit and receive buffer…