Part Number: THVD1429 Dear Technical Support Team,
Upon seeing the input waveform of the DE/RE report, we observed a waveform exceeding the maximum rating for a brief period (less than 10ns).
This duration is likely too short for the IC's body diode…
Part Number: THVD1429 Tool/software: Hello,
My customer has a question for THVD1429.
Does it has UVLO?
They would like to know if there is a possibility to send or receive wrong data when the supply voltage is under recommended operating voltage…
Part Number: THVD1429 Other Parts Discussed in Thread: THVD1450 , THVD1420 , THVD1400 , , SN65HVD23 Tool/software: Hello,
we use two RS-485 transceivers to transmit data with max. 12.288 MHz (differential manchester encoding) over Cat 5e cable. One…
Part Number: THVD1429 Other Parts Discussed in Thread: SN65HVD72EVM Hi Team,
the current test is to use Ti SN65HVD7x EVB *2 and change THVD1429 sample ( only switch DE/ RE, determine the direction), transmit command.
the DUT (STB) on the schematic…
Part Number: THVD1429 Hi Sir,
My customer test THVD1429 in differential output condition as fig. 12 setting. Please check the pic below. During Rising delay on blue line, THVD1429 can't meet datasheet's tr/tf spec. Would you please helping to check…
Part Number: THVD1429 Hello everyone, I have a situation like this: there is a subsystem (around one PCB board, which utilises two MSP430 microcontroller). Subsystem communicates with satellite bus thorugh RS485 bus. Inside the subsystem, these two MCUs…
Part Number: THVD1429 Other Parts Discussed in Thread: THVD1400 , THVD1420 , THVD2410 Hi,
We are using THVD1429DR RS485 IC with CC3220MODSF12MOBR.
We are reading 30 parameters (1 Packet) from slave Device. Frequency: 1 parameter per sec. Baud Rate…
Part Number: THVD1429 Hi Team,
Our customer used THVD1429 on their board but during certification tests, the chip failed at 2kV surge test. The failure mode is short circuit of data+ data- to VCC and GND. I understand that the device can withstand up…
Part Number: THVD1429 Hello Sir,
Per THVD1429 D/S page one show ESD / EFT / Surge protection capability .
Does it mean IC still working normally during these testing ?
Or it just mean IC will not damage only.
Many thanks !