Part Number: THVD1439 Dear TI Support Team,
I have a few questions regarding the internal pull-up and pull-down configurations for the logic input pins (DE, D, and /RE) of the THVD1439 (standard 8-pin separate version, e.g., THVD1439DR).
According…
Part Number: THVD1439 Hi team,
I’m looking for a device similar to the THVD1439 that supports half-duplex communication and includes surge protection. Based on these requirements, is there a TI device that also has an internal termination resistor so…
Part Number: THVD1439 Tool/software: Hi All,
I have a question about THVD1439. Is it necessary to pull up the A(6pin) and pull down the B(7pin)?
Below are the waveforms when each terminal is pulled up and pulled down. The waveform will be normal.…
Part Number: THVD1439 Other Parts Discussed in Thread: THVD1400
Tool/software:
Hello E2E Community,
We seek your inputs & clarification on following queries in regards to the IEC 61000-4-5 Surge testing of the THVD1439
Why is there a 80Ohm coupling…
Part Number: THVD1439 Tool/software: Hello E2E Community,
We are considering the use of THVD1439 Surge Protected TRx for our use case, and are slightly confused about the grounding when using this Surge Protected TRx on our board.
Traditionally we…
Part Number: THVD1439 Other Parts Discussed in Thread: THVD1449 , Hello, is this device robust enough to be used without external TVS diodes protection? If not can you recommend an alternate device
thanks
Part Number: SN65HVD72 Other Parts Discussed in Thread: THVD1439 , Hello Guys,
Good day.
Our customer have used SN65HVD72D in the past but cant find any to buy. Do you know if they can use THVD1439 in the same socket with the surge devices left off…
Part Number: THVD1424 Other Parts Discussed in Thread: MAX3243E , , THVD1454 , THVD1439 , THVD1420 , THVD1520 Hello,
I am designing multiple TI parts into my design, provided that China is not in the pipeline for Country of Diffusion (COD), Country…
Part Number: SN65HVD234 Other Parts Discussed in Thread: THVD1439 , TCAN3414 , SN65HVD231 Tool/software: We want to parallel the A/B output of a THVD1439 and the output of the SN65HVD234 CAN transceiver so either standard could be available on our two…