Part Number: THVD1449 Guten Tag,
im Datenblatt des THVD1449 ist die Beschaltung des /RE-Pins unterschiedlich dargestellt.
Auf Seite 21 ist der Pin mit einem Pull-Up-Widerstand versehen.
Auf Seite 23 allerdings mit einem Pull-Down.
Richtig…
Part Number: THVD1449 Tool/software: Hi,
Is the RFS pull up or pull down needed on A and B pins of THVD1449DR keeping in view the full speed grade and the full length it supports?
Part Number: THVD1449 Other Parts Discussed in Thread: SN65176B Hi team,
I have a customer is testing THVD1449 and have a question.
When Reciever side is Enable and Driver is 0V, the tPZH and tPZL will be 4us and 10us. And they find out that SN65176B…
Part Number: THVD1449 Other Parts Discussed in Thread: ISO3088 , ISOW1432 Tool/software: Hi
I am working on the following RS485 transceiver.
Can you suggest any transformer coupling or any other isolation method to provide galvanic isolation to the…
Part Number: THVD1449 Tool/software: Hello,
in the TI application note " Simplifying Surge Protection for RS-485 Using Integrated Designs " by Parker Dodson it is shown in a block diagram (fig 3-1) that the TVS diodes are integrated in the housing of…
Part Number: THVD1449 Hi team,
Does it have the specific test-mode or -operation, which is out of normal operation, just for final-test or others, and not mentioned in datasheet?
If yes, how does this specific operation mode happen and how to avoid…
Part Number: THVD1450 Other Parts Discussed in Thread: THVD1449 Tool/software: Hi team,
Has this device been evaluated for IEC 61000-4-5? In our circuit, the TVS diode suppresses the voltage to about 53.3V. Simply based on IEC standards, a pulse of…
Part Number: MSP430FR5969 Other Parts Discussed in Thread: THVD1449 , , THVD1406 Tool/software: I was using Back channel (USCI_A0) UART p2.0 and p2.1 for performing serial communication via an rs485. But there is some data integrity issues. So i was wondering…
Part Number: THVD1439 Other Parts Discussed in Thread: THVD1449 , Hello, is this device robust enough to be used without external TVS diodes protection? If not can you recommend an alternate device
thanks
Part Number: THVD1450 Other Parts Discussed in Thread: THVD1420 , THVD1449 , , SN65HVD888 Hello Expert,
We are testing CS (Conduction Immunity) Certification for EMC Test, there is a problem that the communication was cut off, So we are trying to replace…