Part Number: THVD1500 Hi TI team
I wonder if this circuit can satisfy that A signal line and B signal line to GND is 30V (for 30 minutes, the chip temperature does not exceed the maximum temperature).
Will the normal communication be affected if the voltage…
Part Number: THVD1500 Hi,
We are using THVD1500 at 5V. The board is powered using 5V over a connector and we have added a 5V TVS diode at the connector.
The clamping voltage of the TVS diode is around 9.2V whereas the absolute maximum rating of VCC pin…
Part Number: ISO6742 Other Parts Discussed in Thread: ISO6721 , , THVD1500 , ISO6721R , ISO6731 , ISO6741 , ISO1500 , ISO1430 , ISO1450 , ISO1410 Hi experts,
My customer want to realize isolated RS485 through using ISO6742 and THVD1500. But, from my opinion, the…
Part Number: THVD1500 Hi,
To what voltage is RE pin pulled up to?
This pin is connected to our microcontroller GPIO powered using 3.3V. Would this cause 5V to be applied to the controller pin?
Shall we have an external pull up on the pin to 3.3V
Part Number: THVD1500 Other Parts Discussed in Thread: SN74LVC1G34 , THVD1450 , THVD1410 Hi Team,
I am using THVD1500 RS485 transceiver (5V) and interfacing it to a 3.3V level processor.
I am attaching the VOH,VOL,VIH, VIL levels comparision. I found that…
Part Number: THVD1500 Other Parts Discussed in Thread: TCAN1044-Q1 , TCAN1042-Q1 Hi Team,
In my requirement we need to short CAN and RS485 signals in a single line.
Can we connect (CAN_H & RS485_D+) in one line and (CAN_L & RS485_D-) in another line directly…
Part Number: THVD1500 Hi,
Within the datasheet of the THVD1500 the Absolute Maximum Ratings are mentioned. For Vcc this is 7V.
https://www.ti.com/lit/ds/symlink/thvd1500.pdf?ts=1598511064612&ref_url=https%253A%252F%252Fwww.ti.com%252Finterface%252Frs…
Part Number: THVD1500 Hi team,
For Thvd1500, RS485 Bus add pull-down resistance, 3k, A pull up, B pull down. general node less than 20, drive will be ok?
Best regards,