Part Number: THVD1505 Good day Colleagues,
Could you explain if the THVD1505 (or another similar device with auto-polarity correction feature) requires all of the transcievers be supporting this feuture on the bus for proper opeation?
Or any technical…
Part Number: THVD1505 Hi team,
If my customer is using this part as a slave only, not as a master, how does he need to connect the RE_ and DE pins? Do they need to be controlled by the DSP or can they be terminated with a resistor?
Is there a sample circuit…
Part Number: THVD1505 Other Parts Discussed in Thread: SN75HVD06 Dear Sir, Madam,
I would like to use a THVD1505DR for a project but I need more information about it.
- What is the delay between the moment where the component receives data in UART interface…
Part Number: THVD1505 Other Parts Discussed in Thread: THVD1500 , THVD1429 , THVD1510 Team,
just to be sure: THVD1500 can be directly replaced by THVD1505 on an existing PCB designed for THVD1500. Correct? It is 100% backward compatible. Correct?
In fact…
Part Number: THVD1505 Hi Team,
Do we have integrated solution containing both RS-485/CAN interface side? Customer is looking for it. Thanks.
Best,
Stanley
Part Number: THVD1505 Other Parts Discussed in Thread: THVD1426 , THVD1406 Thvd1505 is a non-polar transceiver. Max13487 and max13488 are transceivers with automatic direction selection control. I want to know whether thvd1505 can replace max13487 and…
Part Number: THVD1505 Other Parts Discussed in Thread: SN74LVC1G123 Hi,TI
Our products contain two channels of RS-485 interfaces. In the test, the baud rate of 115200 was used to send data between two channels of RS-485. The test results showed that one…
Part Number: THVD1505
Hi,
There are lots receive issue in our mass products,we didn't found any solder issue, the products can work well if rechange THVD1505DR, and the issue followed with the chip when do cross-validation (A-B-A test). There are 2pcs…
Part Number: THVD1505 Hi,
I can't find any ref design for THVD1505. Customer need this device to support 18KV air-gap discharge. please kindly suggest a ref design to meet this requirement . thanks.