Part Number: THVD1520 Other Parts Discussed in Thread: THVD1420 Hello team,
Customer would like to double confirm if below circuitry is able to apply for THVD1520.
3.3V is for MCU F28377 bias power.
5V is for the RS485 bias power
as we understanding…
Part Number: THVD1520
I have two THVD1520DR connected to each other and with their 120 Ohm resistors at the ends. The problem I have is that the data I send is not received completely, that is, if I send a string of 8 bytes I only receive…
Part Number: THVD1520 Tool/software: Hi Team,
we are using THVD1520 to connect our devices using RS485. the requirement is 3000 feet @ 115200 bps.
do I need send some preamble bytes or sync bytes before I send out the real packet on the RS485 bus…
Part Number: THVD1520 Tool/software: Hi team,
There have several OPNs for THVD1520. I would like to check with you what is the difference and how should we select different OPN?
Thanks!
Ethan Wen
Part Number: THVD1520 Other Parts Discussed in Thread: THVD1426 , Tool/software: Dear Team,
Kindly recommend a circuit to enable automatic direction switching for Transmit and receive.
Also, do I need to pull up the Ro pin, and the DE/RE pin be…
Part Number: THVD1520 Tool/software: I am designing a system with another backup system and these receive the same 485 signal in parallel. This backup system may be unpowered, thus the transceiver would be without supply. Is there a problem with this…
Part Number: THVD1520 Tool/software: Hello team,
At datasheet of THVD1520, we can see below comment
"To eliminate line reflections, each cable end is terminated with a termination resistor, RT, whose value matches the characteristic impedance, Z0…
Part Number: THVD1520 Other Parts Discussed in Thread: SN75176B , Tool/software: Is THVD1520 a drop-in replacement for SN75176B and has better specs than SN75176B ? We are now using SN75176B to interface with the IEbus network in some Toyota/Lexus vehicles…