Part Number: THVD1550 Dear Team,
My customer has used the THVD1550DGKR in their system. They have a question about the Electrical Characteristics under VCC=5.5V to 7.0V. The Electrical Characteristics are defined under VCC=4.5V to 5.5V, but if VCC was…
Part Number: THVD1550 Dear Team,
My customer has used the THVD1550. They would like to know the distribution information for |VOD|. Can you please send it to me?
Best Regards,
Koshi Ninomiya
Part Number: THVD1550 Other Parts Discussed in Thread: SN74LVC1G125
Could I ask about an issue with my current circuit configuration?
Right now, I have two RX lines connected together. Under this condition, when I measure the signal while trying to…
Part Number: THVD1550 Hello guys,
One of my customers is evaluating THVD1550 for their new products.
At this moment, they have the following question. Could you please give me your reply?
Q. They want to avoid the THVD1550 entering standby mode…
Part Number: THVD1550 Other Parts Discussed in Thread: THVD1520 , SN65HVD3088E Hi team,
I have one question as I know SN65HVD3088 is an old part. I suggest THVD1550 to replace the competitor. SP485EEN.
Apart from ESD and speed, what are the differences…
Part Number: THVD1550 Other Parts Discussed in Thread: THVD1500 Hi,
I have related questions for THVD1550: Using THVD1550DR as alternate to DS3695AM/NOPB.
As per the suggestions i have used THVD1500 in the design. Which has signal rate of 500kbps…
Part Number: THVD1550 Hello team,
My customer has some questions related with fail-safe function.
1. When /RE=H, fail-safe in THVD1550 doesn't work, right?
2. Are pin A and B pulled up to Vcc / down to GND in THVD1550, respectively?
Best regards…
Part Number: THVD1550 Other Parts Discussed in Thread: SN65176B , TVS1400 Tool/software: Hi,
What is the signal jitter of THVD1550 at a speed of 10Mbps and a cable length of 100 feet? Is it less than 20%?
According to the documentation, the cables…
Part Number: THVD1550 Hi,
Please tell us about THVD1550. ① Is it digital MOS? Or is it BiCMOS? ② Is it hermetic (airtight sealing structure)? Or is it non-hermetic?
Thank you.