Part Number: THVD1551 Other Parts Discussed in Thread: TPD1E10B06 Hi team,
Could you please help check the schematic as below?
The data frequency is 1~10MHz.
And is it OK by adding common choke in the red square area because the application is motor driver…
Hi Clemens,
You firstly recommend THVD1551 and THVD1451 then you said "the only possible alternatives are the older SN65LBC179A, SN65HVD179, and SN65HVD50". Should I recommend THVD1551 to customer?
Hi MJ,
The THVD1551 is the replacement - (THVD1451 could also work - but generally the more cost effective option is THVD1551). Both of these devices have similar to slightly higher to VOD from the SN65HVD51 so even though they are not labeled high output…
Other Parts Discussed in Thread: THVD1551 , SN65LBC179 Hi all, Good day.
P/N: SN65LBC179QDR
I am creating a delivery specification for this part number. The customer is Panasonic. In the Qualification Summary, the results of ESD-HBM and CDM are described…
Part Number: SN65LBC179 Other Parts Discussed in Thread: THVD1551 , , TPD2E007 Hello,
I have a customer who is looking to use the SN65LBC179Q but needs their solution to meet IEC 61000-4-2 standards. Do you have a recommendation for additional circuitry/parts…
Part Number: SN75176B Other Parts Discussed in Thread: SN74LVC1G07 , , THVD1520 , THVD1426 , THVD1552 , THVD1551 Hi there,
Good day.
This is a product project I'm working on. I want it to be able to provide two different interfaces (RS485 and RS422) and have…
Part Number: THVD1451 Other Parts Discussed in Thread: SN65HVD1474 , SN65LBC179 , THVD1551 Hello team,
I am looking for a TI cross-reference part for the ADM3490 3.3 V, Low Power, RS-485/RS-422 Transceiver (Full Duplex, 10 Mbps)
I have seen both the THVD1451…
Part Number: SN75178B Other Parts Discussed in Thread: THVD1551 , THVD1550 Hi, Good day. Our customer working on the SN75178B and they have the following question: 1. I want know what is the baud rate with this device 2. Is it possible to derive TTL output…
Hi,
We haven't seen similar applications. THVD1451 and THVD1551 are the fastest RS485 TI has. Even the device could take the SDO pulse, the drive might not work due to the bus load. I cannot think of any solution other than stretching the pulses. …
Hi Max,
If I use THVD1551 as a buffer as we discussed earlier by connecting R and D pins externally, what would be the maximum current consumption(supply current+load current) by the IC?
Thanks,
Saumya