Part Number: THVD2450V Other Parts Discussed in Thread: THVD2410V Hello,
For the THVD2410V, the logic inputs (D, DE, RE, SLR) have an absolute maximum rating of VIO + 0.2V.
I have a design where a logic input occasionally experiences brief positive…
Part Number: THVD2450V Tool/software: Dear TI team,
THVD2450VDRCREP
Please provide IBIs model for above part number.
If not available suggest alternate part which has ibis model.
Thanks & Regards, S.Ramakrishna.
Part Number: THVD2450V Hi team,
Customer test IEC61000-4-4 (Fast Transient) test on the communication line.
CUstomer see R pin is toggled to Low from High for 11us even no communication is taken. Actually there were noise on the differential signals…
Part Number: THVD2450V-EP Our team is looking for an RS-422 transceiver that has these specs:
40Mbps
3.3 and 5V input range
30m of cable length
Looking at the datasheet for THVD2450V-EP, it seems it should allow for these specs. However in Figure…
Part Number: THVD2450V Other Parts Discussed in Thread: THVD2450 , TMUX1511 , TS5A3166 Tool/software: Hello,
I was planning to use the THVD2450V RS-485 transceiver because I want to drive the bus at 5V while powering the logic level signals from a 3…
Part Number: THVD2450V-EP Other Parts Discussed in Thread: THVD2450V Tool/software: Hello, I am currently working on designing a system that comprises 7 subsystems. I intend to establish communication between these subsystems using RS485. They will be…
Part Number: THVD2450V Tool/software: For the THVD2450V device, what are the min, typical, max values of the integrated pull-down resistor on the DE pin? On the RE# pin? On the D pin?
Thanks!
Part Number: THVD2450V Tool/software: What is the pressure limit for this part? I am looking to top cool this part with a thermal interface material to a cold plate.
Thanks!
Part Number: THVD2450V-EP Tool/software: Good morning I tried searching for the qualification summary report on part number THVD2450VDRCREP but it says it cannot be found. Can you provide me the qualification summary report?
Tool/software: In my design with the THVD2450VDRCREP RS-485 transceiver, the datasheet suggests using SMAJ30A for surge protection.
Can I replace the SMAJ30A with TPD1E0B04DPL instead?
Will the TPD1E0B04DPL provide adequate protection in this application…