Part Number: THVD4431 Tool/software: I need implement a RS232/422/485 compatible design on one DB9 connector.
The pinout is EIA standard.
I found THVD4431 is perfect for RS232 protocol but totally different pinout for RS422/RS485 protocol.
If TI can p…
Part Number: THVD4431 Tool/software: Hello,
I am currently building a seriel interface with the THVD4431 multiprotocol transceiver in connection with an PCIe UART IC (XR17V354, MaxLinear (former Exar)). The UART IC contains a so called 'auto RS485 half…
Hello Rob,
The TMUX7234 doesn't have powered off protection. Meaning applying a voltage on the source and drain pins with the supply turned off might damage the device. If this is an important part of your design and it can't be altered, I might be able…
Part Number: THVD4431 Other Parts Discussed in Thread: ISOW7742 Tool/software: Hello,
What maximum current does the THVD4431 consume at 5V (worst case)?
I saw 75 mA at 5V. Correct?
I would like to power the THVD4431 with the DC/DC output of the ISOW7742…
Part Number: THVD4431 Hi, i need to know what is the lenght and width of the die from the following component : THVD4431RHA. I am performing fiability test on components and i need to compare the surface aera of the die against the surface aera of the…
Part Number: THVD4431 Tool/software: Hi there,
I'm starting a new design with the THVD4431. I am a bit confused about how to use the V+/V- rails. I guess I am not supposed to apply external power to these inputs, I only need to provide the external…
Part Number: THVD4431 Hello,
We are currently in the process of planning for the integration of the THVD4431 component into our industrial gateway project. In this regard, we kindly request reference schematics for the aforementioned part. Additionally…
Part Number: THVD4431 Hello,
I looked the pinout of the THVD4431 component.
I saw a difference between the THVD4431 datasheet and the evaluation board schematic (THVD4431EVM). Pin 16 is NC in the datasheet and it is symbolized VIO in the THVD4431EVM s…