Part Number: THVD4431EVM Other Parts Discussed in Thread: THVD4431 , TMUX7234 , Tool/software: Hi All
I'm designing a switch between RS232 and RS485 using the TMUX7234 and THVD4431.
Could you please provide their schematics and project? (Altium…
Part Number: THVD4431 Team, Could you please help with the below request?
This card is not functioning as expected: -Board powered by 5V (V+ is approximately 5V and V- is -3V). -we configured it in mode 001 (RS232) and looped L2 back to L3. See attached…
Part Number: THVD4431EVM Tool/software: The eval board doesn't work out of the box. C24 is missing on the board. It is connected to the internal charge pump. After installation it starts working. We bought 2 boards, both had the same problem.
Part Number: THVD4431EVM Tool/software: Hello,
I recently bought the THVD4431EVM. I saw in the user guide that jumpers J28 and J29 need to be set depending on the IC version. Can you tell me if it is a new or an old chip on the picture?
Thanks in…
Part Number: THVD4431EVM Hello,
Would it be possible to have the PDF schematics of the evaluation board? Because the picture in the user's guide is blurry.
Would it also be possible to have the Altium Designer files? Because they will help me in my…
Part Number: THVD4431 Hello,
I looked the pinout of the THVD4431 component.
I saw a difference between the THVD4431 datasheet and the evaluation board schematic (THVD4431EVM). Pin 16 is NC in the datasheet and it is symbolized VIO in the THVD4431EVM…
Hi Chaithra,
So the THVD4431 is pretty straightforward when it comes to application schematics using this device - essentially there are logic I/O that are directly connected to MCU GPIO pins and the bus facing pins (R1 - R8) are connected to the…