Part Number: THVD8000 Hi ,
I am using THVD8000 Driver IC for my new project to power nodes from gateway device over two wire.
The scope of project is
1. Gateway can have maximum of 3 nodes and minimum of 1 node connected on Power over RS485 bus at any…
Hi Jacky,
I have added a few slide decks on the process behind this application as well as a schematic file.
One thing to note is that we didn't build a specific board when testing the application with the THS6222 + THVD8000 - we used already existing…
Part Number: THVD8000 Other Parts Discussed in Thread: TPS62A01
THVD8000接続について質問です I have a question about THVD8000 connection
添付ファイルを見て下さい Please see attached file
電源はTPS62A01を使用します Power supply uses TPS62A01
Fig1はSingle ended connectionです Fig1 is Single…
Hi Sajul,
I apologize for the delay while I was out of office.
1. We don't have a full model - but we do have a simplified PSpice library (can import into any spice software that except HSpice I believe) .
THVD8000.lib
Some notes:
1a) Its a…
Part Number: THVD8000 Hi Team,
Could you please help our customer about their THVD8000 project. We are trying to determine the timings of delays we need prior to sending UART commands via the THVD8000. I had a couple questions.
1. For the switching characteristic…
Part Number: THVD8000 Hi Team,
Our customer wants to use THVD8000 in one 24VAC Air Conditioner power line communication system, below is their schematic for THVD8000 section. Can you help to check if any issues and suggestions? Do we need the pull-up…
Hi Alex,
No worries - 100% understand, end of year business can be a lot!
Understood on the inductors - that makes sense its not uncommon for cost being a driving factor behind higher modulation frequencies.
So if you can run some tests as I previously…
Part Number: THVD8000 Hi team,
My customer have a question.
" o date, our products are powered by 24V DC (+/- 20%) and GND. They communicate in RS485 with the SN65HVD75DGK driver. We could physically remove the RS 485 to pass the data over the power…
Part Number: THVD8000 Other Parts Discussed in Thread: THS6222 Hi folks,
I would have liked to know if it was possible to use coupled inductors for AC coupling with the THVD8000 in order to reduce the number of components on the board (in the case of…
Part Number: THVD8000 Hi
My customer is now using MM1192 as their interface between AC indoor unit and its thermostat, and we would like to see if there is opportunities for TI's devices THVD8000. But due to customers' opinion this two devices are based…