Part Number: TIC12400 I've attached my schematic. HS_LS_IO.pdf I am converting a value on IN10 and it has an offset error. For example:
10V = 10.577
5V = 5.677 etc
From my schematic, if you follow IN1 (upper middle of the page), it goes through…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 When some IN pins of TIC12400 are not used, how to deal with them?
Floating or shorted to GND?
Thanks!
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 Tool/software:
Q1: How to set into polling mode? When we set the CONFIG Register --> POLL_EN=1, but the IC still in continuous mode.
Could you provide the complete polling mode setup…
Part Number: TIC12400-Q1 Hi expert,
Do you have any recommendation for the selection of input series resistance on the input pins of TIC12400-Q1?
Any materials/reference value can help guide customers usage?
Thanks a lot.
BR,
Manu
Part Number: TIC12400 I need to configure IN0 to read a ground or VBAT supply. I have it partially working so let me explain what I am doing.
I enable IN0 (Bit 0, Register 0x1B), next, I leave Register 0x1C Bit 0 to its default which is current source…
Part Number: TIC12400-Q1 Tool/software: Hi,
I am using MSDI-TIC12400QDCPRQ1 in our system. In that we have created a function, by calling it ADC of the particular channel can be calculated. I am facing the issue while calling the function more than…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 , Hi team,
Please check the question below:
Peripheral Circuit:
12V system, the IO pin of TIC12400 is connected in series with a 1kohm resistor to a detection switch, which is then…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 I'm currently wanting to enable the wetting current diagnostics on IN0 of the TIC12400 however when I do this none of the inputs change values anymore if their hardware input states change…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: DRV8718-Q1 Tool/software: Hi BU team,
Have a nice day!
Do you have the output current range of TIC12400-Q1’s SO pin? I can't find it in Datasheet.
Thanks!
Best wishes,
Leo