Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 When some IN pins of TIC12400 are not used, how to deal with them?
Floating or shorted to GND?
Thanks!
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: DRV8718-Q1 Tool/software: Hi BU team,
Have a nice day!
Do you have the output current range of TIC12400-Q1’s SO pin? I can't find it in Datasheet.
Thanks!
Best wishes,
Leo
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 Tool/software:
Q1: How to set into polling mode? When we set the CONFIG Register --> POLL_EN=1, but the IC still in continuous mode.
Could you provide the complete polling mode setup…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400
Tool/software:
Hello,
I have a board with TIC12400-Q1 and esp32-wroom
The schematic:
Like datasheet, i have pull-up's in /INT and CS_n 24V in VS and 3.3v in VDD So, i make…
Part Number: TIC12400-Q1 Tool/software: Per datasheet, The ADC self-diagnostic feature is activated by setting the ADC_DIAG_T bit in the CONFIG register to logic 1. Once enabled, the TIC12400-Q1 periodically sends a test voltage to the ADC. The conversion…
Part Number: TIC12400-Q1 Tool/software: Hi Expert,
when switching from continuous to polling mode, my steps are: SPI write configuration. Set TRIGGER to 0h in the CONFIG register; then POLL_EN to 1h in the CONFIG register, INT_CONFIG to 1h ,POLL_TIME…
Part Number: TIC12400-Q1 Tool/software: Hi,
I am using MSDI-TIC12400QDCPRQ1 in our system. In that we have created a function, by calling it ADC of the particular channel can be calculated. I am facing the issue while calling the function more than…
Part Number: TIC12400-Q1 Tool/software: Hello, I currently have switches connected to inputs IN0 through IN9. When the switches are floating, I observe around 1V. When connected to GND, the voltage drops to approximately 0.8V, and when connected to the…