Hi Pragesh,
Thank you for your patience.
The motor that was used was a 24V/16-pole 3-phase BLDC ceiling fan motor as specified below in the following test results report:
BLDC Ceiling Fan Controller with Sensor-less Sinusoidal Current Control, TIDA-0…
Part Number: UCC28630 Other Parts Discussed in Thread: TIDA-00386 , Hi,
I am looking for a TINA simulation model of UCC28630D. I came across that component from the following link:
Part Number: TIDA-00386
I have downloaded the BOM related to this design and nothing is mentioned related to the part RM10/I : P-1031 5 pin Bobbin. I am looking for the specs related to it. Also, looking for TINA model for the same for simulation purpose…
Part Number: TIDA-00386 Other Parts Discussed in Thread: MSP430FR2111 , DRV10983 Dear Sir,
i want to drive a BLDC motor without Remote controlling feature. So is it possible with 10983 and 10987 Driver IC only. or MSP430FR2111 required for this application…
Part Number: TIDA-00386 Other Parts Discussed in Thread: UCC28630 , DRV10987 , DRV10983 We are looking for development of BLDC fan without remote control operation. Fan speed should be regulated thru custom regulator design and it should be retrofitted…
Part Number: UCC28630 Other Parts Discussed in Thread: TIDA-00386 , , MCF8316A Hi,
We developed a low voltage ceiling fan controller using TI devices.
Power Supply : TIDA-00386 Power Supply (UCC28630), Flyback transformer is Wurth 750343068
Motor Control:…
Hi Mohamed,
You can create circuit for pins like listed below,
SPEED pin-> This is has internal pull down 55Kohm , but you need a speed command. You can use provide resister divider for desired speed since you mentioned constant speed.
SCL/SDA -…
Part Number: UCC28630 Other Parts Discussed in Thread: TIDA-00386 , MCF8316A ,
We developed a low voltage ceiling fan controller using all TI devices.
Power Supply : TIDA-00386 Power Supply no changer, Flyback transformer is Wurth 750343068
Motor Control…
Part Number: DRV10983 Flyback Transformer Datasheet Discrepancy
Hello,
I am working on a BLDC motor driver using the DRV10983. In the application note it refers to a transformer that is used in the AC-DC to generate 24VDC from AC mains input. Here is…