TI E2E support forums
TI E2E support forums
  • User
  • Site
  • Search
  • User
  • E2E™ design support >
  • Forums
    • Amplifiers
    • API solutions
    • Audio
    • Clock & timing
    • Data converters
    • DLP® products
    • Interface
    • Isolation
    • Logic
    • Microcontrollers
    • Motor drivers
    • Power management
    • Processors
    • RF & microwave
    • Sensors
    • Site support
    • Switches & multiplexers
    • Tools
    • Wireless connectivity
    • Archived forums
    • Archived groups
  • Technical articles
  • TI training
    • Tech days
    • Online training
    • Live events
    • Power Supply Design Seminar
  • Getting started
  • 简体中文
  • More
  • Cancel


Search tips
Showing 12,975 results View by: Thread Post Sort by
    • 8/29/2025
    • Carson Wang

    TIDA-010243: TIDA-010243: Calibrator about TIDA-010243,MSPM0

    Part Number: TIDA-010243

    Tool/software:

    Regarding calibration parameters for TIDA-010243:

    1. Macro definitions in “template.h”:

    PHASE_A_VOLTAGE_SCALE_FACTOR  xxxx.x

    PHASE_A_CURRENT_SCALE_FACTOR  xxx

    How are these values calculated based on this schematic? Could you provide a specific formula and calculate the result? Our configuration parameters:ADS131M08 value:OSR=1024  Gain=1  SAMPLE_RATE=4000

     

                                         

    1. I understand that each phase requires calibration of six parameters. My question concerns the correspondence between the macro definitions in” template.h” and the parameters shown in the diagram below. I only need to know the parameters for phaseA.

    I don't know which value in the chart each one corresponds to.

    #define PHASE_A_VOLTAGE_SCALE_FACTOR                1585.2

    #define PHASE_A_CURRENT_SCALE_FACTOR                125

    #define PHASE_A_POWER_SCALE_FACTOR                  (PHASE_A_VOLTAGE_SCALE_FACTOR * PHASE_A_CURRENT_SCALE_FACTOR)

    #define PHASE_A_VOLTAGE_DC_ESTIMATE                 100

    #define PHASE_A_CURRENT_DC_ESTIMATE                 0

    #define PHASE_A_VOLTAGE_AC_OFFSET                   0

    #define PHASE_A_VOLTAGE_FUNDAMENTAL_OFFSET         0

    #define PHASE_A_CURRENT_AC_OFFSET                   0

    #define PHASE_A_CURRENT_FUNDAMENTAL_OFFSET         0

    #define PHASE_A_ACTIVE_POWER_OFFSET                 0

    #define PHASE_A_ACTIVE_POWER_FUNDAMENTAL_OFFSET    0

    #define PHASE_A_REACTIVE_POWER_OFFSET               0

     

    Thanks

    Carson

     

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 11/10/2025
    • Larry Ciscon

    TIDA-010938: TIDA-010938.5 variant differences?

    Part Number: TIDA-010938

    We'd like a bit of clarification about how the variants work.  We're interested specifically in the TIDA-010938.5 configration/variant.  How do we build this specific version?  Do we need a different BOM?  Are there any differences in the PCB?

    Any/all info would be helpful.

    Thanks in advance.

    Power management forum Power management
    • 10/13/2025
    • Ali Movahedi

    TIDA-010239: TIDA-010239

    Part Number: TIDA-010239

    Tool/software:

    Yes, I have a similar question.  I was wondering if this reference design is not still available for purchasing or borrowing from TI, please.

    Thanks.

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 12/9/2025
    • Abhishek Sathyendran

    TIDA-010265: Compilation Errors After Importing TIDA-010265 Project

    Part Number: TIDA-010265

    Hello,

    I recently imported the TIDA-010265 reference design project into Code Composer Studio. I have not made any changes to the code, but when I try to build the project I receive several compilation errors.

     

    In addition, many source files and header files in the Project Explorer are marked as Excluded. 

    Could you please advise on:

    1. Why several files are automatically excluded from the build after importing the TIDA-010265 project?

    2. How to correctly re-enable the necessary files or restore the original build configuration?

    3. Whether there is a specific CCS version or compiler version required for this reference design.

    I have attached the screenshot of the errors and the excluded files for reference.

    image.png

    image.png

     

    Thank you.

    Arm-based microcontrollers forum Arm-based microcontrollers
    • 9/30/2025
    • Mahammad Kasim

    TIDA-010232: TIDA-010232

    Part Number: TIDA-010232

    Tool/software:

    HVDC live and return path.

    In our 800 V HVDC network, we have implemented a resistor divider network on the line path, but not on the return path since no negative supply is available from the source. However, in the reference design, resistor divider circuits are used on both the positive and return paths for insulation monitoring. We would like to confirm whether our approach is correct, or if the HVDC return path also requires a resistor divider network.

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 9/26/2025
    • James Peverill73

    TIDA-01606: TIDA-01606

    Part Number: TIDA-01606

    Tool/software:

    I am trying to prototype the TIDA-01606 reference design. It appears that the old revision (E6) has now been taken down. The new revision does not appear to have BOM files in XLS format or pick n place files. Are these going to be posted at some point? It is difficult or impossible to prototype the board without these. Thank you! 

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 9/25/2025
    • Shailendra Pardeshi

    TIDA-010057: TIDA-010057

    Part Number: TIDA-010057

    Tool/software:

    Hello, I am looking for design files for TIDA-010057: Swaroop board. Do let me know how can I get it?

    Regards,

    Shailendra.

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 11/5/2025
    • Ali Movahedi

    TIDA-010239: Searching for TIDA-010239 Board

    Part Number: TIDA-010239

    Dear TI Team,

    We are into a new design and we were wondering if we could buy or borrow the TIDA-010239 EVC Evaluation Board.  I would also appreciate it if I could be directed where I can purchase one.

    Thanks, ALi.

     

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
    • 12/3/2025
    • jason chen29

    TIDA-050089: TIDA-050089 test board gerber file support???

    Part Number: TIDA-050089

     

    Hi Team 

    can help me 

    Could you help me obtain the Gerber for the test board used in the module?

    Snap93.png

    Power management forum Power management
    • 9/20/2025
    • M Ranjith Rai

    TIDA-010265: TIDA-010265

    Part Number: TIDA-010265

    Tool/software:

    Im currently working TIDA-010265 based design and as per the guide i need to change the DMC_BUILDLEVEL in the sys_settings.h file which is by default DMC_LEVEL_4, but when i build the project it automatically come back to default DMC_LEVEL_4. what is the issue here

    Simulation, hardware & system design tools forum Simulation, hardware & system design tools
>

Didn't find what you are looking for? Post a new question.

  • Ask a new question