Hi all,
When I am debugging a program I am getting the following message. What might be the chances for data bytes not being written?
PS: All input voltages and hardware setup has been verified correctly.
Message:
MSP430: Loading complete. There…
Hi, Mohammed,
The schematic is OK.
Since one device works well, I think it's probably the code is not correct.
Here are the TLC5971 code for TIDA-00979:
Fullscreen
4135.3113.TLC5971.c
Download
#include "TLC5971.h"
// Initialisation…
Hi, Suresh,
We don't have the Embedded C reference source code.
But you can refer to the following TI designs using TLC5971:
RGB LED Signal Tower With Wi-Fi® Interface Reference Design: www.ti.com/.../TIDA-00994;
RGB LED Signal Tower for Industrial…