Part Number: TIDA-010056 Other Parts Discussed in Thread: MSP430FR2355 , MSP430FR4133 , , DRV8350R , DRV8353 Hello TI Helpers,
I'm using CCS version 10.1.1.00004 . I have MSP430FR4133 launchpad used as burner into my controller which has MSP430FR2355…
Part Number: TIDA-010056 Hi Team, we would like to seek your assistance.
The firmware(TIDA-010056) is not compiling properly on CCS.
Thank you in advance.
Regards,
Mark
Part Number: TIDA-010056 Dear
The reference design shows the possibility to measure the back EMF.
The measuring is mentioned in the documentation but the resistors are marked as DNP in the schematic.
Since I dont have a clue about the processor and so…
Part Number: MSP430FR2355 Other Parts Discussed in Thread: TIDA-010056 , DRV8350
Tool/software: Code Composer Studio
For TIDA-010056 application code whether both open loop control and closed loop control is implemented, for initial start up which type…
Part Number: TIDA-010056 Hello,
I am wondering why R1, C13, R2, C14, R3, C15 are DNP but R14, C16, R15, C17, R16, C18 are placed. Is that because a voltage surge in the high-sde MOSFET is not as serve as that in the low-side MOSFET? or is that design…
Part Number: TIDA-010056 Other Parts Discussed in Thread: TPS709 , TLV767 Hello. I am planning to design a 48V, 1kW BLDC drive for my college project based on the TIDA-010056. I have a couple of simple questions
1. The reference design uses a two stage…
Part Number: TIDA-010056 I have a question about Operating Ambient. I guess it is limited to +55C because the design does not have any heatsink. And if we add heatsink it will go to +85C. Correct? Why is it limited to -20C? Which part limits the temperature…
Hi, Alex,
1. It would be difficult to use F280049 launchpad with TIDA-010056. If you really want to use the launchpad, I suggest you to use DRV8353EVM. Please refer to
2. If you want to continue to setup the TIDA-010056, please send me the 1) Error page…