HI Dennis ,
yes i still working on the project of water meter~
but now i have switch the design from TI MSP430 ESI to TI CC1310 one TIDA-01228 "Low-Power Water Flow Measurement With Inductive Sensing Reference Design"
link : www.ti.com/.../TIDA-01228…
Other Parts Discussed in Thread: CC1310 , TIDA-01228 Dear Sir,
I have asked some question about the tidud25a before,
recently, i need to go implement more test on it ,
my test board was CC1310 Launchpad and custom LC board (mainly refer to the…
HI M-W,
Sorry for the delay.
My main goal is make the SCS project work in the sensor/collector
my file is attached belore
All my work at now are based on the reference design, let me
1) the TIDA-01228 from the SCS
to_ti_LC_sensor_tida01228…
Jeff,
It would be good if you use the HELP function in the Sensor Controller Studio and teh documentation of th efunctions (see bottom right: Available procedures window and do a double click), which describes all functions, triggers and so on - this…
Part Number: CC1310 Other Parts Discussed in Thread: TDC1000 , Hi community members,
Would you please help me to locate reference design of CC1310 with TDC1000(ultrasonic)
Similar to below design which is with LC sensor
www.ti.com/.../TIDA-01228…
Jeff,
I’m really happy to read that you finally have your solution running and the distance of 4 to 4.5 mm is what I achieved as well and documented in the TIDA-01228. So you confirm my findings, which is good!
Now, increasing the gap to 6 or 7 mm…