Other Parts Discussed in Thread: TIDA-01571
Dear Team, Do you have the DMD Flex Cable design or Gerber files for TIDA-01571?
I couldn't find them on the website.
Thanks for your support!
Best,
Johns
Part Number: DLP3010 Other Parts Discussed in Thread: TIDA-01571 , DLPDLCR3010EVM-G2 Tool/software: Dear Team, Since I didn’t get a response from the other side , I might have posted in the wrong place, so I’m posting again here. Where can I obtain the…
Part Number: TIDA-01571 Tool/software: Hello,
When I try to download the gerber files at this link TIDA-01571 reference design | TI.com , the resulting zip file is corrupted and cannot be opened or extracted. Maybe this is linking to the wrong file…
Part Number: TIDA-01571 Hi,
there is a similar question like this, but for the generation 1 model:
My goal is the same: I want to trigger a camera synchronized to the VSYNC of the projector.
Now there does not seem to be a test point on the boards…
Hi Michael,
Thank you for your interest in DLP Technology!
In the DLPDLCR3010EVM-G2 User Guide Table 1, these values can be found.
Throw ratio 1.2
This means if you wish to project an image that is 16" wide, the projector would have to be 19…
Hi Silvio,
We do not have a complete, ready-to-use projection module that contains all the devices you listed.
The closest we can offer is the DLPDLCR3010EVM-G2 , which has the DLP3010, DLPC3433, and DLPA3000. There is a reference design, the TIDA…
Hello Thomas,
They can find the schematics for the board detailing routing and test points here: https://www.ti.com/tool/TIDA-01571 . They may need to remove the heat sink to gain access to some of these test points. Otherwise at least for the first…
Hello Jessie,
Thanks for the information.
Could you please try to check two things.
1.) Please check the DMD voltages which are Vofs, Vbias, Vreset
2.) Please check the LEDs and see if you see any current or voltage.
You can find the following…
Hi Vladimir,
Please use the following links to review the reference designs:
DLPDLCR3010EVM-G2: https://www.ti.com/tool/TIDA-01571
DLPDLCR3010EVM-G1: https://www.ti.com/tool/TIDA-00384
DLP3010EVM-LC: https://www.ti.com/tool/TIDA-080003
Regards…
Hello Michael,
Welcome to DLP forum and thank you for your interest in DLP technology.
Please refer to the following reference design:
www.ti.com/.../TIDA-01571
regards,
Vivek