Part Number: TPS65987D Other Parts Discussed in Thread: TPS65987 , TIDA-050012 , TIDA-050014 , TPS65981 Hi ,
I have same issue in TPS65987 ,
When I set 20V 3A profile to 20V 5A. by Source Board(TIDA-050012) with pjt(TIDA-050012 Source Board)
Then using Sink…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS65987 , TIDA-050012 , TPS65981 Tool/software: TI C/C++ Compiler Hi ,
I have same issue in TPS65987 ,
When I set 20V 3A profile to 20V 5A. by Source Board( TIDA-050012 ) with pjt(TIDA-050012 Source Board…
Hi ,
I have same issue in TPS65987 ,
When I set 20V 3A profile to 20V 5A. by Source Board( TIDA-050012 ) with pjt(TIDA-050012 Source Board)
Then using Sink Board( TIDA-050014 ) to Check Source Profile with "Received Source Capabilities(0X30)",
But the…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS65981 , TIDA-050012 Hi Team,
We are evaluating TPS65987DDH at the following condition.
Then, source board supply 5V and around 800mA at source and sink capability 5V/0.9A so correct behavior.
…
Part Number: TPS65988 Other Parts Discussed in Thread: TIDA-050012 , Hi team,
Customer have some question about customization tool.
They would like to know how to configure PWM driver (GPIO14, 15)
when you open TIDA-050012 template file, you can see HW…
Q1: The easiest way to to this is to create a new project targeted at the TIDA-050012 Source Board. This is the power duo source board and it will configure the switches to meet your requirements.
You do need to configure the device as a UFP (Device…
Part Number: TPS65987D Other Parts Discussed in Thread: TIDA-050012 , TPS65981 , , Using the TPS65981 Application customization tool, I tried to program the TPS65987DDH/Standard/Downstram Facing Port/ configuration onto the TIDA-050012 DUO Source Board.…
Then you can use the PWR DUO Sink configuration template as an example. Please refer to my previous post, but instead of clicking TIDA-050012 Source Board, you would click on TIDA-050012 Sink Board.
You would the virtual devices to advertise its sink capabilities…
And if I instead of Standard or Advanced when setting up New Project select TIDA-050012 Source Board, then I get a Device 1 tab and can select Device 1 Port 1 when importing, but then an Exception occurs.
Exception Encountered during Import From Device…
Part Number: TPS65987D Other Parts Discussed in Thread: TIDA-050012 Hello,
Is it realistically possible to run TPS65987D at 20V and 5A and deiliver 100W without a FET?
How much heat needs to be dissipated in this case?
Thank you and best regards,
Ambr…