Ying Liu said: 1. Rs state: No current is set. And how to set it?
2. Ramp up state: Current Shoot when change to next state. Why is like that?
Please provide the spec. of the motor and the user.h you used.
Ying Liu said: 3. Rated Flux state: The motor stop…
Part Number: DRV8306 Hi, currently i'm working on the design of a bldc module control. I found DRV8306 interresting for my application but my question is can this IC control BLDC motor without hall sensor (I think no) ? Thank's for your time, B…
Part Number: TIDA-01102 Hi,
I am designing a board using a printed coil matrix inspired by the TIDA-01102. I am now looking into how to design the ground planes for the board.
Looking at the TIDA-01102 design, I am struggling to understand why there…
Part Number: TIDA-01513
Hi Expert,
Good day!
We are checking this TIDA-01513 . Would this be suitable for isolation system for48v system?T he reference design has a solid state relay IC.
If not, can we get a reference design for isolation system suitable…
Part Number: TIDA-060029 Hi Team,
Base on the TIDA-060029 ref design. The customer wants to measure 500pF~1nF capacitance and frequency around 2MHz.
How to choose OP spec or other devices to achieve the function? Customers need a fully total solution…
Part Number: DRV8701EVM Other Parts Discussed in Thread: TIDA-00875 , DRV8870 HI,
I have read the reference design TIDA-00875.
And I have used the DRV8870 to drive the single-phase BLDC.
But I had a problem with the motor starting itself in certain positions…
Part Number: TMS320F280049 Other Parts Discussed in Thread: PMP23126 , TIDM-02000
Hi expert,
I have seen some peak current control reference design using C2000 by internal DAC and comparator, that's good actually however could I learn that if any fully…
Hi,
LM5170's AGND and PGND should be connected together.
LM5170 is capable of generating negative voltage output from +/- 12V input voltage. What is the negative voltage output?
Best Regards,
Feng Ji
Part Number: DRV8300DIPW-EVM Other Parts Discussed in Thread: LAUNCHXL-F280049C , Hi,
Planning to Test DRV8300DIPW-EVM + LaunchXL-F280049C - BLDC 6 step motor control Solution on our 2 wheeler Hub motor.
Speed reference has to be from a Potentio Meter (…
Part Number: TIDA-00176 Other Parts Discussed in Thread: TIDA-01629 , TIDA-010025 Hi team,
My cusotmer finds that this app note is for AC motor. Do we have such an app note for synchronous motor?
Thanks!