Part Number: TIDC-CC2650STK-SENSORTAG Other Parts Discussed in Thread: CC2650 , CC2640R2F I am looking to purchase this device but looking to add support for an external sensor. The device description suggests that it can be expanded. I cannot seem to find…
As such, TISDK builds for AM335x EVMs are provided here :
http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Overview_Building_the_SDK.html
We, are in the process of updating the wpa-supplicant recipes here to make MESH as a default configuration…
Part Number: TIDC-WL1837MOD-AUDIO-MULTIROOM-CAPE Other Parts Discussed in Thread: TMDXEVM3358
Hi Team,
Hardware: BEAGLEBK TIDC-WL1837MOD-AUDIO-MULTIROOM-CAPE
Software: PROCESSOR-SDK-LINUX-AM335X V06.00 AM335xBluetopiaLinuxProduction
I have some question…
Part Number: TIDC-WL1837MOD-AUDIO-MULTIROOM-CAPE Hi
I wonder if it is possible to share the schematic file for the WiLink 8 Wi-Fi Bluetooth Smart Audio Multiroom Cape CAD Files.
I find shematic in PDF, and also CAD files for the PCB board. But non shematic…
Part Number: CC2650STK
Hi TI Experts,
Please let me confirm my question.
[Question] According to the User's guide and wiki, the SensorTag battery is not necessary if the sensortag revsion 1.3 or later. Is this description correct?
TI wiki: processors…
Hello,
If you disconnect the mmWave sensor and have only the DCA1000, then plug in the 5V 3A power source and flip the switch to the position that lights up the LEDs, do you see the four DevPack ports then?
Best Regards,
Pedrhom
Part Number: TLV320AIC3104EVM-K Tool/software: Hello,
I have followed the procedure in SLAU855A to install the AIC310x GUI on my Windows 11 laptop. When I connect a USB cable to the AC-MODEVM carrying the AIC3104 EVM, I see the USB ready (D1) and power…
Part Number: TAS2781EVM Other Parts Discussed in Thread: TAS2781 Tool/software: We've been granted access to PurePath Console, in order to build a product with TAS2781.
The eval board seems to be properly connected to the PC. But not audio output…
Hello,
"I am using the latest version of the SDK, ti-processor-sdk-linux-am62xx-evm-10.00.07.04. Even without editing the DTS file, I connected the MAX30102 sensor. However, the issue is that the sensor connects intermittently, and I have shared the images…