Part Number: TIDM-01000 Other Parts Discussed in Thread: C2000WARE , CCS version : 20.3.1
DIGITAL POWER SDK : C2000Ware_DigitalPower_SDK_5_06_00_00
MCU : F28379D
Board : TIDM-01000
S/W : pfc3phvienna_F2837x
In debugging Graph display value is…
Part Number: TIDM-01000 Other Parts Discussed in Thread: TIDM-1000 Regarding the TIDM-1000..
Is this design using Park and Inverse Park transforms to do the control of inner and outer control loops?
Is Clarke transform involved?
Can the Power Factor…
Part Number: TIDM-01000 Hi,
we use the contol card of the TIDM 1000 for a 20000kW PFC. All builds were done now and we want to check the over and undershoot at load changes. Is the correction factor for the non linear voltage loop always active or…
Part Number: TIDA-010000 Other Parts Discussed in Thread: C2000WARE , TIDM-01000 CCS version : 20.3.1
DIGITAL POWER SDK : C2000Ware_DigitalPower_SDK_5_06_00_00
MCU : F28379D
Board : TIDM-01000
S/W : pfc3phvienna_F2837x
I launched compansation…
Piyush -
I am also not sure about our entire portfolio on this - perhaps someone else could chime in -
if it helps or you can change the sensors or the architecture of your design in any way - i could point you to this reference which uses MSP430FR2355…
Hi U-SK,
While it might be possible to implement the HART modem in software, we don't have any references at the moment.
In addition to the TI Design TIDM-01000 mentioned by Mitch above, TIDA-01504 might also be a good resource. It uses a DAC8740H…
Part Number: DAC161S997 Other Parts Discussed in Thread: MSP430FR2355 , TIDA-00648 , TIDM-01000
Good morning,
I have some issues with the communication between the MCU MSP430FR2355 and the DAC161S997.
My goal is to simply program the current that…
Lori,'
Thanks for your reply, I have read the encoder spec that you sent and compare with a format spec. And I also adjusted for number of bits and crc...... in source code library and try to test with a format encoder, but communication between MCU…