Part Number: TIDM-02014 Other Parts Discussed in Thread: TIDM-02010 , TIDA-010265 Tool/software: Dear Experts,
I want to use the Motor Control GUI for the TIDM-02014 project but in the GUI I cannot choose this project (only one), see the photo below…
Part Number: TIDM-02014 Other Parts Discussed in Thread: OPA320 Tool/software: Hi TI expert,
In TIDM-2014, Could you please explain the circuit below:
Why Voutput is in range 0.33 to 2.97V?
Thank you
Part Number: TIDM-02014 Tool/software: Hi TI Team,
We are using TI Rev B and Rev C of WS Inverter - Ctrl Board. I have a question related to the LEM current sensor +/-15V supply. We see NT400 in the schematic, but it's not in the BOM and assembly drawing…
Part Number: TIDM-02014 Tool/software: Hello E2E Experts,
Good day.
Do we have a 15kW, 48V inverter for 3 wheeler application?
If none, is there any way to convert existing traction inverter reference design to 12kW to 15kW?
Regards,
TI-CSC
Part Number: TIDM-02014 Tool/software: Hello,
As per the block diagram on TIDM-02014, is mentions about a "Safety MCU"
so my question is which of the above cards is used as MCU in this reference design as both the cards are mentions in the document…
Part Number: TIDM-02014 Other Parts Discussed in Thread: TMS320F280039C , SYSCONFIG , C2000WARE , TMS320F280049C , TMS320F280039 Dear Experts,
I am porting the TIDM-02014 code coded in TMS320F280039C to TMS320280049C. As a result of the overall investigation…
Part Number: TIDM-02014 Tool/software: Dear all, thanks for reading
I would like to know if there's a chance to acquire the design files created for the reference designs.
Assuming there's a mechanism to get them I would like to discuss such a possibility…
Part Number: TIDM-02014 Other Parts Discussed in Thread: UCC14240-Q1 , LM5158-Q1 , LM5157-Q1 Tool/software: Dear Experts,
1. I would like to ask is a simple boost converter is recommended (can be used) instead of the SEPIC LM5158QRTERQ1 that was chosen…
Part Number: TIDM-02014 Hello, I am trying to run a 3 phase motor of (Maximum DC voltage 800V, Maximum Motor Terminal Voltage 530V(L-L), Rated current(rms) 300A, Peak current(rms) 400A, Rated power 250 kW, Peak power 300kW). My questions are: 1. Do we…
Part Number: TIDM-02014 Hello,
I am working with TIDM-2014 product with TIDM-02014_traction_inv_F28003x software.
I have some questions about the software. 1-
pwm1.Vabc_pu[0] = 0.5; pwm1.Vabc_pu[1] = 0.5; pwm1.Vabc_pu[2] = 0.5; when I change it…