Hi Ryan,
Please make sure all the jumpers are correctly populated as mentioned in the 'hardware setup' section of the TMDSHVRESLLCKIT user guide. Please check that you are getting the 5V and 3.3V on the base board. The fact that you run into similar issues…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: TIDM-DELFINO-ETHERCAT , CONTROLSUITE , TMS320F28379D , TMDSCNCD28379D Hello everyone :)
It's my pleasure to be here and this is my first post. Well, I have a problem. I have this launchpad: www…
Part Number: EMB1428Q We are referred to “TIDM-TMS570BMS” to do the design. (But on EMB1428Q PIN48 is empty and on EMB1499 CELLPLUS is not used.)
1. EMB1428:
- Issue 1:
There are three boards. On two of them no matter what to do the PIN source…
Hi Margarita,
I am using DM3730 EVM with default bootargs and psp04.02.00.07.sdk.
I faced same problem when run the command:
./decode -v /usr/share/ti/data/videos/davincieffect_480p30.264 -O lcd / tv
I followed your suggestion to solve this issue but when…
Garrett,
If you are concerned specifically about the EtherCAT solution, there have not been updates to that kit since v3.4.7 of controlSUITE. Attached is the release notes for the latest release. Let me know if you still have any concerns.
Release…
Part Number: TMDSICE3359 Other Parts Discussed in Thread: LAUNCHXL-F28379D , AM4379 , TIDM-DELFINO-ETHERCAT
Hello,
I successfully launched EtherCAT master project with Acontis master stack on tmdsice3359. I used that document from TI:
My simple network…
Please see
We currently do not have a 3.6kW LLC, but do have the PFC design with 3.6kW
Additionally if for LLC interleaving is required we have the below design to demonstrate the controller capability
Hi,
You are right. The coefficients should be treated as Q26 numbers. I believe this is a bug. This is an older design and I would recommend referring to our latest LLC solution below.
I hope this helps.
Hrishi
Hi Kun,
For the PFC part you can refer to the following designs:
For the DC-DC part you may refer to the following designs, although the voltage levels for these designs are different than the ones you mention. We are working on a similar DC-DC design…