Part Number: TIDM-02010 F280025_ODU_SCH pfc.pdf
Hi TI team,
The attached Circuit is our PFC circuit in our ODU design. At max load, we are facing a issue in the PFC circuit. When i am driving the Compressor motor to max 320 Electrical Hz, i am able…
Part Number: PMP22650 Other Parts Discussed in Thread: TMDSCNCD280039C , We are using the TMDSCNCD280039C control card. When we directly inject a 50 Hz AC signal with a 1.65 V DC bias into the TTPLPFC_VAC pin, all six PFC drive signals are output normally…
Part Number: TMS320F280039 Other Parts Discussed in Thread: TIDM-02013 Dear TI Experts,
I'm currently studying the TIDM-02013 project, and I'm confused about the calculation of the instantaneous current reference value required for the PFC current loop…
Part Number: TIDM-1000 Other Parts Discussed in Thread: POWERSUITE , C2000WARE Tool/software: Hello,
For debugging purpose, I would like to use DAC that are available on TIDM-1000 PFC evaluation board, on connector J5 :
In PowerSuite SW I think…
Part Number: TIDM-02010 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi,
According to the TIDM-02010 Schematic, the RC values for Vac are as follows:
Cs (Input Capacitance): 6.8 nF
Rs (Input Resistance): 150 Ohms
When using…
Part Number: TIDM-02010 Other Parts Discussed in Thread: SFRA Tool/software: Hi Experts,
We are developing a board inspired by the TIDM_02010_DMPFC design. Currently, we are tuning the PFC’s current loop using the SFRA tool. While analyzing the function…
Part Number: TIDM-02010 Tool/software: Hi Experts,
We are using a reference design for our PFC proof-of-concept (POC). However, after removing the EPWM_setPeriodLoadMode function call to enable access from the shadow register, we observed unexpected…
Part Number: TIDM-02010 Tool/software: Hi,
I am seeking documentation that explains the calculation of IacRef, particularly the role of pfcVars.VinvSqr, which is causing some confusion.
Additionally, I would greatly appreciate any documents or resources…
Part Number: TIDM-02002 Tool/software: Hi,
We are currently considering whether it is possible to digitally control a power system consisting of a three-phase AC input followed by PFC and DC/DC conversion.
We are planning to use separate MCUs to independently…
Part Number: TIDM-02013 Hi,
There are 2 totem pole topologies.
1. interleave totem pole (used in TIDm-02013)
2. Totem-Pole Bridgeless PFC (Diode Rectification)
My question is can we use T otem-Pole Bridgeless PFC (Diode Rectification) for bidirectional…