Hi,
I'm looking to build led driver that powers directly from main AC (90-230VAC), the LED's:
32 LED's (3-4V each, can be in series/parallel/mixed)
2 to 10A adjustable current
1 to 5 msec pulse duration
up to 60 pulses/sec
Please help…
Part Number: TIDM-02002 I have a project would be use C2000 to implement the 10kW Bidirectional AC/DC converter for Automotive application, but I have one question what would be the auxiliary power in the bidirectional converter? if I need to do the auxiliary…
Other Parts Discussed in Thread: TPS92513 , LM3445 Please heip to suggest LED driver solution and spec as below : Vin : 90 ~ 264Vac Vout : 6 ~ 36Vdc Iout : 0.35A_Constant Current. ( ±5%) Target Topology : single stage both PSR or SSR is ok.
B/R Jam…
Part Number: IWR6843ISK Hi,
I'm facing the same problem as the person in this forum
https://e2e.ti.com/support/sensors/f/1023/t/846748?IWR6843ISK-Cannot-connect-to-COM-Port#pi320995=1
My board was bought on 26.12.2018, so I'm guessing its a…
Part Number: TMS320F280049C Other Parts Discussed in Thread: TIDM-1007 Tool/software: Code Composer Studio Dear Sir,
About the project of Design Guide: TIDM-1007, TIDU61B.
1) The first phase current IL1 is routed to CMPSS1, then from CMPSS1_CTRIPH_OR_L…
Part Number: IWR1443BOOST Hi gents,
when I have everything connected, the PC fails to detect the COM Port from the EVM board. also the yellow led which is the nRST led does not turn on. It used to work fine. it just happened to me today. Anyone had…
Part Number: TIDM-MSP430AFE253SUBMETEREVM Other Parts Discussed in Thread: MSP430AFE253 , MSP430I2041 , EVM430-I2040S Hello,
I was reviewing the TI design of the single phase energy meter using built in AC/DC converter, and as per the schematic the…
Part Number: TPS92410 Other Parts Discussed in Thread: TPS92411 Hello Team,
For TPS92410 and TPS92411,
Can this solution be used for universal input supply range?
Can this support design up to 30W?
What is max conversion efficiency achieved…
Part Number: TPS92210 I looking for below LED driver condition.
・Input:415V AC/DC
・Vout and Iout:TBD
・Need to 0%~100% dimming control
If there match device, please let me know.
Or, I think that close solution is PMP6023, is there way to use…