Part Number: UCC24624 Other Parts Discussed in Thread: UCC24612 Tool/software: Hello,
I have been going through some other controllers for a synchronous rectifier such as UCC24612 and I noticed that they have calculations for the minimum RDS(ON) of the…
Part Number: UCC28600 Other Parts Discussed in Thread: UCG28826
Tool/software:
Hello,
I am currently working on a project to design a GaN-based Power Factor Correction (PFC) and Quasi-Resonant (QR) controller. My specifications include an output power…
Hello Tushant,
Please see my comments below .
I am not sure if this code is shareable with customers or not.
My suggestion is that you can simply run own your code on small microcontrollers like MSP devices.
As per the Hw schematic between the Test automation…
Part Number: AM6422 Tool/software: Hi Ti Team,
I have built the mcu app (ipc_rpmsg_echo_linux) for r5fss0-0_freertos based on the sdk 9.02.
It can start from the linux side, but after running, stop the remote core will get timeout.
Here is the log for…
Hello Charles, The XOR that the FAQ and the TRM both refer to, just describes how the device loads up the programmed OTP values. This BQ76952 OTP FAQ answers what are they key things to be aware for OTP programming with our device. As mentioned previously…
Part Number: TMP421 Other Parts Discussed in Thread: DXP Tool/software: Hello,
I want to confirm I am connecting and using an appropriate PNP transistor for remote sensing with the TMP421. I selected a 3906 PNP transistor, where I connected the emitter…
Part Number: TIDM-02014 Tool/software: Dear all, thanks for reading
I would like to know if there's a chance to acquire the design files created for the reference designs.
Assuming there's a mechanism to get them I would like to discuss such a possibility…
Part Number: UCC27282 Tool/software: Hi Team,
Do we have recommended DC to AC solution for driving PDLC?
Input voltage is 5VDC supplied from adapter. Output requirement: AC output voltage ~40VAC, output power ~10W.
Could you please check whether the…
Part Number: TIDM-02012 Tool/software: Are there any updates regarding dynamic vibration compensation algorithm on the Mathworks model like disucussed here: ? e2e.ti.com/.../tidm-02012-model-files---dynamic-vibration-compensation
Ashik,
This is a very generic question. We have PWM examples, which you could then use to control each half bridge.
I think a better route would be for you to look through our digital power reference designs: https://dev.ti.com/tirex/explore/node?node…