Part Number: TIDM-RESLLC-DCDC Tool/software: Hi.
I am trying to learn about resonant converter and I understand the theory how the circuits behaves, the different regions. However, I have a hard time to understand the control implementation. I always…
Part Number: TIDM-RESLLC-DCDC Other Parts Discussed in Thread: TIDM-02002 , TIDM-1001 We design step-up power module, DC48V input, output 90V, power 2000W, output with constant current and short circuit protection。Select the output up to 60V or 72V by…
Part Number: TIDM-RESLLC-DCDC Other Parts Discussed in Thread: CONTROLSUITE Hello, I'm interested in buying the product: TIDM-RESLLC-DCDC In order for me to order it I need the electrical simulation in PSPICE to show it to my teacher that the simulations…
Part Number: TIDM-RESLLC-DCDC Hi team,
I'm working on a power supply DC/DC isolated and resonant, 24VDC input, 12VDC output, power will be around 200W/300W; do you believe the TIDM-RESLLC-DCDC could work also at these lower Vin?
If not, could you…
Part Number: TIDM-PSFB-DCDC Tool/software: Dear TI experts,
Recently I am searching a DCDC which has very low Rth_ja , because the output power dissipation is very high , could you help to recommend one suitable DCDC.
The detail requirement as follows…
Part Number: TIDM-PSFB-DCDC Tool/software: Hi,
Is there a full-bridge isolated DCDC solution that can be implemented under the above conditions with both the primary and secondary sides full-bridge?
- Input 40V-100V - Output 25-50V
Probably a solution…
Other Parts Discussed in Thread: TIDM-PSFB-DCDC Tool/software: Helllo,
I would like to implement the following using SEPIC topology.
- Vin: >1.8V
- Vout: 12~24V(variabel)
- Iout: 0.5A
Please recommend DCDC
Best Reagard
SON
Part Number: TIDM-02000 Other Parts Discussed in Thread: TMS320F280039 ,
Tool/software:
Hello,
I develop PSFB DCDC converter.
I use reference design TIDM-02000 and use TMS320F280039 MCU.
When DCDC turn on, Main Trans. 1st current peak current…
Part Number: TIDM-02000 Tool/software: Hello.
I have a question about slope campensation in TIDM-02000.
I can set RAMPMAXREF value.
But I can not see slope operation.
Can I see slope waveform using oscilloscope?
Thanks,
Sangmo Kim…