Part Number: LP5812
Hi,
I am currently evaluating a new RGB LED driver and came across the LP5812 , which seems to fit my application well.
My application requires:
3 RGB LEDs, and
1 additional white LED
All LEDs should be independently…
Part Number: LP5812 Hello E2E Experts,
I would like to confirm that configuring the LP5812 with common cathode RGB is supported.
Like the image below.
Regards,
TICSC
Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLP4710 Hello TI Team,
I am working on converting a DLPDLCR4710EVM-G2 evaluation module into a standalone Spatial Light Modulator (SLM) for an optical experiment using an external laser…
Part Number: BQ25895 Hello,
I am evaluating the BQ25895 for a 1S Li-ion (3300mAh, 5A discharge capable) powered system.
Application details:
• Input: 5V wall adapter, up to 3A available • Battery: 1S 3300mAh Li-ion • Load: 5V rail powering 80 RGB…
Part Number: DLP4500 Hello, I am requesting technical support regarding the LightCrafter 4500. I am currently using the LightCrafter 4500 with an external LED light source as a DMD-based projector. I am now trying to evaluate and use the internal LED…
Part Number: LP5030 Tool/software: Hi,
In the DS we have brightness control for each RGB LED. But, I'm planning to drive 30 white LEDs from LP5030. I need individual LED brightness control.
Is it possible in LP5030 (by setting colour register values…
Part Number: DLPC3479 Tool/software: Hello TI,
If Red LED Max Current[5Ch] = 767(12A) is set and Red LED Current[54h] = 1023(16A) is set, what happens? Does DLPC3479 return something of errors?
Regards,
Uryyy
Part Number: LP5009 Other Parts Discussed in Thread: LP5018 Tool/software: Hi,
We have a exisitng design based on LP5009 driving 3 RGB LEDs.
We want to update the design to drive 6 RGBs in total using LP5009 as shown below. Please review the schematics…
Part Number: BQ34Z100-G1 Tool/software: We are currently in the process of designing a battery-powered system that incorporates the BQ34Z100-G1 fuel gauge. One of our key requirements is to control an RGB LED based on the battery status. The LED in use…