Part Number: DLPC3479 Tool/software: Hello TI contact,
I tried Green LED=0 and Blue LED = 0 of the Write RGB LED Max Current (5Ch) because green and blue LEDs are disable. However, Read RGB LED Max Current(5Dh) return both 91. Why does the case occur…
Part Number: LP5812 Tool/software: Hi Jared,
I would like to get Linux drivers for the RGB LED Driver part - LP5812ADSDR as well, I saw you share the driver link, could you kindly tell me how can i access the link ?
Thanks
Steven
Part Number: TPS929240-Q1 Other Parts Discussed in Thread: TLC6C5712-Q1 Tool/software: I am designing an LED control schematic featuring a common-anode RGB LED. Is it possible to control the RGB LED using the circuit shown in the provided below link …
Part Number: DLPDLCR471TPEVM Other Parts Discussed in Thread: DLP4710EVM-LC Tool/software: Would like to use this DLP engine with 532nm or 660nm laser light and input a controllable sequence of 2D monochrome images. Does TI offer this module with everything…
Part Number: DS16EV5110 Tool/software: Dears:
Customer want to have a device that can adjust LED screen RGB parameter , As sometimes they change LED Screen vendor , different vendor has different performance . Thanks .
Part Number: DLPC3479 Other Parts Discussed in Thread: DLPA3005 , DLP4710EVM-LC Tool/software: When I set 00h to 5Bh using the DLPC3479's "Write RGB LED Current PWM (54h)" command and read it back, the set value becomes 5Bh. Why is that? The DLPA3005…
Part Number: LM3697 Other Parts Discussed in Thread: TLC5973
Tool/software:
Hi TI team.
LM3697 is specified for three-string white LED driver but we wanna use it for a three-string RGB LED, is it possible?
If not possible, what part you recommend…
Part Number: TPS929240-Q1 Tool/software: I am developing a prototype for CHMSL.
We will be using 37pcs Osram RGB LEDs (KRTBDWLM32.32) .
Each LED has a current of 10/50 mA.
Is it okay to run 8 LEDs (24 ports) on the TPS929240-Q1?
When the LEDs…
Part Number: LM3466 Tool/software: Hi,
I'm looking for suitable RGB strip LED driver.
Strip LED voltage = 12V
576 LEDs
70W / roll ( so, 70W / 12V = 5.83A total)
Each color or each channel (For example Red) color will draw about 1.94A
Do you…
Part Number: LP5521 Other Parts Discussed in Thread: LP5810 , LP5562 Tool/software: Hello everyone, Thank you for your time.
I'm the co-founder of a startup where we create LoRa communication boxes for SAR missing person services.
I've recently started…