Other Parts Discussed in Thread: INSTASPIN-BLDC , DRV8301 , CONTROLSUITE Hi All,
I purchase DRV8301-HC- EVM Rev D board (Serial No D1A_1512079), I am able to control the Board through the InstaSpin GUI, but now i want to perform the same operation though…
Part Number: MSP430FR2355 Other Parts Discussed in Thread: TIDA-010056 , Tool/software: Code Composer Studio Hi,
I was going through the code for sensorless control of BLDC using MSP430fr2355 as mentioned in design guide TIDA-010056. Here in design guide…
Garrett,
If you are concerned specifically about the EtherCAT solution, there have not been updates to that kit since v3.4.7 of controlSUITE. Attached is the release notes for the latest release. Let me know if you still have any concerns.
Release…
Other Parts Discussed in Thread: BOOSTXL-DRV8301 , MOTORWARE , DRV8301 , LAUNCHXL-F28027F Hello,
I'm working on driving a BLDC motor, in a sensorless mode, with the duty cycle of PWM that I will generate from an external device, with its own algorithm…
Hi Whitney,
Hi Chris,
thanks for answer! I have solved my Problem. I am using a type uint8_t and i am thinking that type has a size of 8 Bit but it has a size of 16bit. So i overwrite memoryspace i have not reserved before. I am changing the typdef
fro…
Other Parts Discussed in Thread: DRV8301-69M-KIT , INSTASPIN-BLDC , MOTORWARE , CCSTUDIO , INSTASPINUNIVERSALGUI , DRV8301 , UCC27524 , TMDSHVMTRINSPIN , TMS320F28069M , UCC27322 , TMS320F28069F Hello, I need help choosing the best evaluation kit for our electric…
Other Parts Discussed in Thread: DRV8301 , INSTASPIN-BLDC , CONTROLSUITE , MOTORWARE Hello,
I would like to make a BLDC driver with F2806x MCU and DRV8301 driver. The BLDC driver has to be UL certified.
So I'm testing DRV8301-HC-EVM rev D kit with F28069M…
Part Number: DRV8305 Other Parts Discussed in Thread: MSP430G2553 ,
Hello sir,
I have used DRV8305 and an MSP430G2553 controller to drive BLDC.
It runs almost perfectly but at some point of time BLDC motor internally make a sound for a second and that…
Other Parts Discussed in Thread: DRV8301 , DRV8313 , DRV8332 Hello,
I recently completed a test that required control of eight BLDC motors (48V/5A/10k RPM) using eight DRV8301-HC-C2-KIT eval boards running lightly modified Instaspin software and a Stellaris…
What is the voltage? I'm going to assume if 200W you are probably at 12 or 24V. The HVMTR+PFC is 50-350V bus, 10A. What I would suggest is the DRV8301-HC-C2-KIT. This is up to 60V, 60A and also includes the F28035.
The included projects with this…