thanks james for your answers,
1/ about the first question that what i though at first, but i want to make sure.
so the more resistor i use the less risk i got when one of them got shorted.
2/ concerning the second question, i went to the new EVM TIDM…
Hello,
Previously I was using IAR KickStart license and hence I was getting the code size error before but now I have the IAR full version and now the code is building properly.
In the TIDM GUI folder it was suggested to use GUI associated to an i2040…
Other Parts Discussed in Thread: MSP430I2041 , TIDM-3OUTSMTSTRP , EVM430-I2040S Hi Expert,
May I know if we have solution like PL7413 which is suitable for smart plug/strip application?
Thanks.
Allan
Hello,
To be safe, I would recommend using isolators between the Linux host and the i20xx device. Like I mentioned above, there are certain scenarios where you don't have to do this, such as when there's no wired connection from the host processor to…
Hi Art,
Art Mecina said: Customer have already tried to flash some default images to the EVMi2040, however after flashing the image he cannot see any results from the development board. LED indicators are working but he cannot receive any message from…
Part Number: MSP430I2041 Other Parts Discussed in Thread: MSP-EXP430F5529LP , UNIFLASH , MSP430F5529 , TIDM-3OUTSMTSTRP , MSP430F67791A , TIDM-3PHMTR-TAMP-ESD , EVM430-F6779 , MSP430F67791 , MSP-ISO , EVM430-I2040S , MSP-FET I use Software EMDC ver 1.140.00.03…
If you do not need display, then you do not need high pin count uC. Anyway you cannot run decent web server on any msp430, so you need low-end uC (i-series?) for metering and some ARM for webserver. I would go for http://www.ti.com/tool/TIDM-TWOPHASEMETER…
Hello Abhay,
Have you seen the following resources ? The application note and design guide have some valuable information on how to setup and calibrate the i2040 for this application type.
www.ti.com/.../TIDM-TWOPHASEMETER-I2040
www.ti.com/.../evm430…
Hello Suman,
Please note that the MSP430F425 is not recommended for new designs (NRND) and has been replaced by the MSP430F425A . You can look at some of our E-Meter EVMs to try to reason out how it is down on those chips.
Such as:
www.ti.com/..…
Hello Anuparm,
We do offer an Energy Library that can help with this, but I am unsure if it is available for this part. I know it is not the same part, but the following resources have parts with similar modules that can help you with this.
www.ti…