Part Number: TIOL112 Tool/software: Hello Support Team,
I would like to know if it is possible to use the TIOL 112 without NFAULT being received by the microcontroller in charge of the IO-Link communication. Is there any special recommendation for…
Part Number: TIOL112 Other Parts Discussed in Thread: TIOS102 Tool/software: Hello:
We are considering TIOL112 as a general purpose DIO for a DAQ (24V capable). Do you see any issues with this approach? The thought here is to have one pin that can be…
Part Number: TIOL112 Other Parts Discussed in Thread: TIOL111 , Hello,
I want to confirm if there is any difference in reverse polarity function between TIOL111 and TIOL112.
While the TIOL111 datasheet says “Reverse Polarity Protection of up to…
Part Number: TIOL112 Dear Specislists,
My customer is considering TIOL112 for original protocol and has a question.
I would be grateful if you could advise.
---
TIOL112 is used as a transceiver to communicate between devices using a original protocol…
Part Number: TIOL112 Hi team,
Do we have a component that can support the IO-link without needing an external clock?
Thank you.
Kind regards,
Wouter Kragt
Part Number: TIOL112 Hi team,
My customer want to use TIOL112 as IO-link(When EN=H) and PNP digital input(When EN=L).
Since TIOL112 doesn’t have a current sink for PNP digital input, we want to use ILLM CQ discharge feature of IO-link master mode…
Part Number: TIOL112 Hello Support team
My customer inquires TIOL112 questions, could you support?
*NFAULT support the followign three items, is this correct? 1)UVLO on both L+ and VCC_IN 2)Thermal warning 3)Over current
*"Figure 8-3. Device State…
Part Number: TIOL112 Hi team,
My customer is checking TIOL112's behavior.
In push-pull mode, when they change the state of EN and TX from EN=H, TX=L(=>CQ=L+) to EN=L, TX=L(=>CQ=Hi-Z), the CQ output voltage has a step at 3~4V, then fully discharged…