Part Number: TIOL1123 Other Parts Discussed in Thread: ISO6763 , TIOL112 Tool/software:
Hi,
I need a help to TIOL1123 circuits
TIOL1123 Vout doesn't work
VCCOUT Pin = 0V
I don't understand where I'm making the mistake.
We built 2 boards and…
Part Number: TIOL1123 Tool/software: Hi Team,
I received the following questions from my customer.
Is the component TIOL1123DRCR is washable?
Can you please confirm this?
Thank you.
Kind regards,
Wouter Kragt
Part Number: TIOL1123 Other Parts Discussed in Thread: TIOL1113 Tool/software: Hi,
We use TIOL1123 as output, output mode is NPN,
circuit is shown as below:
When EN is high, CQ is normal, 0V. When EN is low, CQ is about 4V at the beginning…
Part Number: TIOL1123 Other Parts Discussed in Thread: SN65HVD101 , , TIOL112 , TIOL111 , SN65HVD102 Hi, we use SN65HVD101 IO-Link PHY for our IO-Link devices. We consider switch to TIOL1123. There are some differences between these transceivers and differences…
Part Number: TIOL1123 Other Parts Discussed in Thread: TIOL1125 , TIOL112 Hai,
we want implement IO-link interface feature in our products for that we need IO-link device transceiver IC, Please suggest IO-link device transceiver IC and microcontroller…
Part Number: TIOL1123 Hello,
regarding to the datasheet page 19, TIOL1123 is capable of withstanding up to 1.2 kV of 1.2/50 – 8/20 μs IEC 61000-4-5 surge with a source impedance of 500 Ω.
IEC61000-4-5 states to use 2, 12 or 42 Ω as source impedance…
Part Number: TIOL1123 Other Parts Discussed in Thread: BOOSTXL-IOLINKM-8 , TIOL112 , LP-AM243
Hello,
From the datasheet and EVB I see it's possible to run this TIOL1123 as an IO-link master transceiver. Does TI have a way for us to evaluate this IC…
Part Number: TIOL1123 Other Parts Discussed in Thread: TIOL112 , BOOSTXL-IOLINKM-8 Hi,
I want to read and write data from IO-Link device that is a sensor to measure Temperature and Flow rate. The Microcontroller can not directly connect to IO-Link device…